About ACLK_CLK_ROOT of i.MX6Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ACLK_CLK_ROOT of i.MX6Solo

562件の閲覧回数
yuuki
Senior Contributor II

Dear all,

I refer to the "Figure 18-2. Clock Tree - Part 1" of Reference Manual.

ACLK_CLK_ROOT is listed, but I was not able to find the module which used this clock with a reference manual.

Is this clock used in i.MX6Solo?

If this is not used, can I leave the related register the default?

Best Regards,
Yuuki

ラベル(1)
タグ(1)
0 件の賞賛
2 返答(返信)

459件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mx6solo use this clock, one can set it through CCM_CSCMR1 register.

detailed information, one can refer to the Figure 18-8. of Reference Manual.

0 件の賞賛

459件の閲覧回数
yuuki
Senior Contributor II

joanxie

Dear Joan Xie-san,

Thank you for an answer.

However, I cannot find a peripheral using ACLK_CLK_ROOT.
Which peripheral is ACLK_CLK_ROOT used for?

Best Regards,
Yuuki

0 件の賞賛