About ACLK_CLK_ROOT of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ACLK_CLK_ROOT of i.MX6Solo

627 Views
yuuki
Senior Contributor II

Dear all,

I refer to the "Figure 18-2. Clock Tree - Part 1" of Reference Manual.

ACLK_CLK_ROOT is listed, but I was not able to find the module which used this clock with a reference manual.

Is this clock used in i.MX6Solo?

If this is not used, can I leave the related register the default?

Best Regards,
Yuuki

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

524 Views
joanxie
NXP TechSupport
NXP TechSupport

mx6solo use this clock, one can set it through CCM_CSCMR1 register.

detailed information, one can refer to the Figure 18-8. of Reference Manual.

0 Kudos
Reply

524 Views
yuuki
Senior Contributor II

joanxie

Dear Joan Xie-san,

Thank you for an answer.

However, I cannot find a peripheral using ACLK_CLK_ROOT.
Which peripheral is ACLK_CLK_ROOT used for?

Best Regards,
Yuuki

0 Kudos
Reply