Hi community.
Our customer has three camera interface questions.
1, IMX6DQ Reference Manual also YUV 10bit input on the might describes that which can be inputted using the Parallel.
Would you tell me the specific pin assignment?
Below understanding is correct?
I refer Description of IMX6DQAEC of 4.11.10.1 IPU Sensor Interface Signal Mapping of YCbCr 20bit in.
IPUx_CSIx_DATA00 = C [0]?
...
IPUx_CSIx_DATA19 = Y [9]?
2,CAMERA RAW mode data will become the only input in the MIPI?
Is it possible input even Parallel?
Although RAW mode is transferred to the memory space is available, but the process of the data needs to be driver software .
Would you can decoder to the video with an image converter on the hardware?
3,RAW data Would IMX6DQ support manufacturer, etc.?
Does it can be use as the input image the RAW data of Toshiba Image sensor?
已解决! 转到解答。
Hi Takashi
1. yes understanding is correct
2. for MIPI formats one can look at Table 19-1
Regarding "can decoder to the video with an image converter on the hardware" -
this is too vague question to answer reasonably.
3. no, specific manufacturer formats are not supported
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi
1. yes understanding is correct
2. for MIPI formats one can look at Table 19-1
Regarding "can decoder to the video with an image converter on the hardware" -
this is too vague question to answer reasonably.
3. no, specific manufacturer formats are not supported
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------