APBH register of i.MX6Dual.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APBH register of i.MX6Dual.

Jump to solution
975 Views
takashitakahash
Contributor III

Dear community.

Our customer has question below.

Regarding the APBH register, since it is booting with NOR FLASH in the customer system, is there no doubt that this register is not set?

Thank you,

Best Regards.

T.Takahashi.

Labels (1)
0 Kudos
1 Solution
833 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

APBH is used with nand as shown on Figure 14-1. AHB-to-APBH Bridge DMA Block Diagram

i.MX6DQ Reference Manual so ROM initializes it only for nand boot.
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
834 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takahashi

APBH is used with nand as shown on Figure 14-1. AHB-to-APBH Bridge DMA Block Diagram

i.MX6DQ Reference Manual so ROM initializes it only for nand boot.
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos