Build toolchain according to "i.MX Yocto Project User's Guide" in "5.1.2. Setup aarch64 toolchain" section of AN12195
When I run "bitbake core-image-base", I get a lot of errors (some are excerpted below)
Do you know the solution?
I. -include ../git/localedef/include/always.h -Wall -Wno-format -c -o ld-collate.o glibc/locale/programs/ld-collate.c
| In file included from /usr/include/x86_64-linux-gnu/bits/types/locale_t.h:22:0,
| from /usr/include/string.h:152,
| from ../git/localedef/include/string.h:1,
| from glibc/locale/programs/ld-address.c:25:
| /usr/include/x86_64-linux-gnu/bits/types/__locale_t.h:28:8: error: redefinition of ‘struct __locale_struct’
| struct __locale_struct
| ^~~~~~~~~~~~~~~
| In file included from glibc/locale/langinfo.h:591:0,
| from glibc/locale/programs/ld-address.c:24:
| glibc/locale/xlocale.h:27:16: note: originally defined here
| typedef struct __locale_struct
| ^~~~~~~~~~~~~~~
| In file included from /usr/include/x86_64-linux-gnu/bits/types/locale_t.h:22:0,
| from /usr/include/string.h:152,
| from ../git/localedef/include/string.h:1,
| from glibc/locale/programs/ld-address.c:25:
| /usr/include/x86_64-linux-gnu/bits/types/__locale_t.h:42:33: error: conflicting types for ‘__locale_t’
| typedef struct __locale_struct *__locale_t;
| ^~~~~~~~~~
| In file included from glibc/locale/langinfo.h:591:0,
| from glibc/locale/programs/ld-address.c:24:
| glibc/locale/xlocale.h:39:4: note: previous declaration of ‘__locale_t’ was here
| } *__locale_t;
The i.MX Yocto Project User's Guide has recommended minimum Ubuntu version.Please check the i.MX Yocto Project User's Guide you refering and install all packages refering the 3.2 Host packages.
Hi Qmiller
My development environment is:
Ubuntu 18.04.1
Yocto L4.9.51
AN12195 application note mentions Yocto version L4.9.51,
Is it better to use Ubuntu 20.04 and the latest Yocto?
Or is it better to use Ubuntu14.04?
Best Regards
Hi Qmiller,
I tried it on Ubuntu 16.04.7, but the following error occurred when executing the "repo init" command
unxp@U16047:~/imx-yocto-bsp$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-morty -m imx-4.9.51-8mq_beta.xml
Downloading Repo source from https://gerrit.googlesource.com/git-repo
repo: Updating release signing keys to keyset ver 2.3
Traceback (most recent call last):
File "/home/unxp/imx-yocto-bsp/.repo/repo/main.py", line 38, in <module>
from color import SetDefaultColoring
File "/home/unxp/imx-yocto-bsp/.repo/repo/color.py", line 18, in <module>
import pager
File "/home/unxp/imx-yocto-bsp/.repo/repo/pager.py", line 63
sys.exit(f'fatal: cannot start pager "{pager}"')
^
SyntaxError: invalid syntax
unxp@U16047:~/imx-yocto-bsp$
Best Regards
Tried on Ubuntu 20.04.5, repo init completes without issue.
However, when I run "bitbake core-image-base", I get the following error.
#error "Please port gnulib freadahead.c to your platform! Look at the definition of fflush, fread, ungetc on your system, then report this to bug-gnulib."