AMP mode support for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMP mode support for i.MX6

708 Views
ramansubramania
Contributor I

It does not look like AMP mode is standard in all i.MX6 processors.  Is
that correct?

I don't see it in the datasheets or reference manuals, so
I am guessing that

most i.MX6's don't have AMP mode.  The confusion comes
because there are  websites which refer to the AMP ability with i.MX6
processors.

Can you please clear up this issue?

Labels (1)
0 Kudos
1 Reply

378 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raman

NXP supports i.MX6SX running linux + mqx, also please look at

MX6D example

https://community.freescale.com/docs/DOC-94513

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos