ADV7180 for CM-FX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADV7180 for CM-FX6

891件の閲覧回数
madstrum
Contributor III

Hi,

I'm using CM-FX6 from Compulab and a custom baseboard.

I realised that I may need the adv7180_tvin.ko driver to get tv input for the baseboard.

How can I go about doing this?

Sorry I'm a newbie to arm chips in general, so please forgive me if this is a dumb question.

Thank you.

0 件の賞賛
返信
3 返答(返信)

604件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mad

please check links below

Patch to support adv7180 TVin chip for Freescale Android R10.4 BSP on iMX53 -blog archive

Re: ADV7181 on IMX6Q board

How to test TV-IN ( ADV7180) for IMX53 ARD board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

604件の閲覧回数
madstrum
Contributor III

HI Igor,

Thanks.

If I use Yocto to build the linux image using the instructions in the freescale bundle, will the driver adv7180_tvin.ko be included in? 

0 件の賞賛
返信

604件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mad

for adv7180 one needs to use unit-test program : mxc_v4l2_tvin

for yocto:

L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code

Best regards

igor

0 件の賞賛
返信