Hi There I can't figure out how to get the ADC to work on the IMX6SX. I have tried the following so far:
inlcuded the imx6sx.dtsi that creates the adc1 reference as follows:
adc1: adc@02280000 {
compatible = "fsl,imx6sx-adc", "fsl,vf610-adc";
reg = <0x02280000 0x4000>;
interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6SX_CLK_IPG>;
num-channels = <4>;
clock-names = "adc";
status = "disabled";
};
I have enabled adc1 in my own dts file as follows:
&adc1 { vref-supply = <®_vref_3v3>; status = "okay"; };
I have both the IMX7D and the vf610 adc driver compiled in my linux kernel
But I can't see any devices unde /sys/bus/iio/devices
Can somebody tell me what am I missing?
Best regards,
Jeroen van der Laan
已解决! 转到解答。
Hi Jeroen
please try procedure given in Chapter 53 ADC Driver
attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jeroen
please try procedure given in Chapter 53 ADC Driver
attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
This procedure does provide me with an sysfs entry in /sys/devices/soc0/soc/2200000.aips-bus/2280000.adc with the following contents:
./power
./power/control
./power/runtime_active_time
./power/autosuspend_delay_ms
./power/runtime_status
./power/runtime_suspended_time
./driver_override
./modalias
./subsystem
./of_node
./uevent
I'm missing the in_voltage0_raw~ in_voltage3_raw sampling_frequency_available and in_voltage_sampling_frequency entries. Does it have anaything to do with setting the ADC pin settings?