Hi,
I am working on ADC of imx6ul. I have to read 8-ADC input, other than resistive touch intput and USB ID pin.
There is only 10 ADC channels available out of that 6 channels are already used in resistive touch(4 channel) and USB ID pin(2 channel). Now As my requirement is to read more 8-ADC input.
Is it possible to assign ADC input on other port?
Thanks
Hi Jignesh
only available adc muxing options are provided in
i.MX6UL Reference Manual Chapter 4 External Signals and Pin Multiplexing
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
If more channel are needed one may consider external analog multiplexer.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------