I tried to use the ADC on IMX6ULL EVK without success.
I followed the cap 56 on the linux reference manual anabling the devide driver for Freescale vf610 ADC driver but I don't se the devices ...
/sys/devices/soc0/soc.1/2200000.aips-bus/2280000.adc/iio:device0:
/sys/devices/soc0/soc.1/2200000.aips-bus/2284000.adc/iio:device1:
but in /sys/devices/soc0
I have only soc directory with 2200000.aips-bus but without any adc directory inside
/sys/devices/soc0/soc/2200000.aips-bus
drwxr-xr-x 7 root root 0 Jul 19 05:04 .
drwxr-xr-x 12 root root 0 Jul 19 05:04 ..
drwxr-xr-x 3 root root 0 Jul 19 05:04 2280000.dcp
drwxr-xr-x 3 root root 0 Jul 19 05:04 2284000.rngb
drwxr-xr-x 3 root root 0 Jul 19 05:04 2290000.iomuxc-snvs
drwxr-xr-x 3 root root 0 Jul 19 05:04 2294000.snvs-gpr
-rw-r--r-- 1 root root 4096 Jul 26 08:02 driver_override
-r--r--r-- 1 root root 4096 Jul 26 08:02 modalias
lrwxrwxrwx 1 root root 0 Jul 26 08:02 of_node -> ../../../../firmware/devicetree/base/soc/aips-bus@0220000
drwxr-xr-x 2 root root 0 Jul 26 08:02 power
lrwxrwxrwx 1 root root 0 Jul 19 05:04 subsystem -> ../../../../bus/platform
-rw-r--r-- 1 root root 4096 Jul 19 05:04 uevent
Any idea?
Thanks
Fabio
I add the following lines in the DTS file
&adc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_adc1>;
num-channels = <5>;
status = "ok";
};
&iomuxc {
imx6ul-ccimx6ul {
/* Uncomment specific pins of the ADC channels enabled in 'adc-ch-list' */
pinctrl_adc1: adc1grp {
fsl,pins = <
/* GPIO1_4/ADC1_IN4 (pin 7 of the expansion header) */
MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0x80
>;
};
};
and the compile to obtain the DTB file and included it in the boot configuration
So now I see under soc.0/soc/2100000.aips.bus
the device 2198000.adc and nothing else
It is different from the manual but it seem something ...
Any suggestions to go ahead and see something also under /sys/bus/iio/devices?
Thanks
Hello,
please check the dts file, if adc is enabled; by default it is disabled.
imx6ull.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
imx6ul.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Regards,
Yuri.
I checked and it is disabled ....
But also changed don't solve the problem ... it seems to be not used the dtsi file
or problably I have to clean something in order to recompile
How is the sequence to change and reconfigure the project with new dtsi file?
thanks
Hi,
I enabled the clock and now I'm able to read/write the ADC registers.
But always I don't se the correct programming interface ...
/sys/devices/soc0/soc.1/2200000.aips-bus/2280000.adc/iio:device0:
/sys/devices/soc0/soc.1/2200000.aips-bus/2284000.adc/iio:device1:
but only /sys/devices/soc0 with inside
drwxr-xr-x 9 root root 0 Jan 1 1970 .
drwxr-xr-x 9 root root 0 Jan 1 1970 ..
drwxr-xr-x 4 root root 0 Jan 1 1970 backlight
-r--r--r-- 1 root root 4096 Aug 5 12:22 family
-r--r--r-- 1 root root 4096 Aug 5 12:22 machine
drwxr-xr-x 2 root root 0 Aug 5 12:22 power
drwxr-xr-x 4 root root 0 Jan 1 1970 pxp_v4l2
drwxr-xr-x 6 root root 0 Jan 1 1970 regulators
-r--r--r-- 1 root root 4096 Aug 5 12:22 revision
drwxr-xr-x 12 root root 0 Jan 1 1970 soc
-r--r--r-- 1 root root 4096 Aug 2 14:24 soc_id
drwxr-xr-x 7 root root 0 Jan 1 1970 sound
drwxr-xr-x 4 root root 0 Jan 1 1970 spi4
lrwxrwxrwx 1 root root 0 Jan 1 1970 subsystem -> ../../bus/soc
-rw-r--r-- 1 root root 4096 Jan 1 1970 uevent
Any suggestions?
in general one can also look at MX6ULL FreeRTOS adc examples in
sdk/boards/evkmcimx6ull/driver_examples/adc
"Windows installer - MCUXpresso SDK2.2 for i.MX 6ULL"
Best regards
igor
Hi,
the DEMO release does not start ... while also the release coming with the EVK the memtool doese not work
root@imx6ull14x14evk:~# /unit_tests/memtool ADC1.HC0.ADCH
SOC: i.MX6ULL
ADC1 Addr:0x2198000
ADC1.HC0 Addr:0x02198000 Value:0x0000001F - ADC_HC0 can be used for both software and hardware trigger mode.
ADC1.HC0.ADCH(0..4) :0x1f
This 5-bit field selects one of the input channels.
root@imx6ull14x14evk:~# /unit_tests/memtool ADC1.HC0.ADCH=0x0
SOC: i.MX6ULL
write 0x00000000 to Bit 0..4 of 0x02198000
root@imx6ull14x14evk:~# /unit_tests/memtool ADC1.HC0.ADCH
SOC: i.MX6ULL
ADC1 Addr:0x2198000
ADC1.HC0 Addr:0x02198000 Value:0x0000001F - ADC_HC0 can be used for both software and hardware trigger mode.
ADC1.HC0.ADCH(0..4) :0x1f
This 5-bit field selects one of the input channels.
There is some protected areas where is not possible to modify the registers?
Thanks
Fabio
Hi Fabio
one can try Demo Images Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dua
and follow sect.4.1.6 Programming Interface Linux Manual included in Linux L4.14.98_2.0.0 Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks Igor,
I already saw this chapter ... but in my system I have this directory contents
root@imx6ull14x14evk:/sys/devices/soc0/soc/2200000.aips-bus# ls -la
drwxr-xr-x 7 root root 0 Jul 26 06:35 .
drwxr-xr-x 12 root root 0 Jul 26 06:35 ..
drwxr-xr-x 3 root root 0 Jul 26 06:35 2280000.dcp
drwxr-xr-x 3 root root 0 Jul 26 06:35 2284000.rngb
drwxr-xr-x 3 root root 0 Jul 26 06:35 2290000.iomuxc-snvs
drwxr-xr-x 3 root root 0 Jul 26 06:35 2294000.snvs-gpr
-rw-r--r-- 1 root root 4096 Jul 26 10:13 driver_override
-r--r--r-- 1 root root 4096 Jul 26 10:13 modalias
lrwxrwxrwx 1 root root 0 Jul 26 10:13 of_node -> ../../../../firmware/devicetree/base/soc/aips-bus@0220000
drwxr-xr-x 2 root root 0 Jul 26 10:13 power
lrwxrwxrwx 1 root root 0 Jul 26 06:35 subsystem -> ../../../../bus/platform
-rw-r--r-- 1 root root 4096 Jul 26 06:35 uevent
and not
/sys/devices/soc0/soc.1/2200000.aips-bus/2280000.adc/iio:device0:
/sys/devices/soc0/soc.1/2200000.aips-bus/2284000.adc/iio:device1:
(honestly I didn't jave soc.1 directory ...)
I have to enable the ADC in someway?
I confirm I'm not abel to write the internal register with memtool
root@imx6ull14x14evk:/unit_tests# ./memtool 2198014 1
E
Reading 0x1 count starting at address 0x02198014
0x02198014: 00000200
root@imx6ull14x14evk:/unit_tests# ./memtool 2198014=0x20f
Writing 32-bit value 0x20F to address 0x02198014
root@imx6ull14x14evk:/unit_tests# ./memtool 2198014 1
E
Reading 0x1 count starting at address 0x02198014
0x02198014: 00000200
root@imx6ull14x14evk:/unit_tests#
the value does not change!