Hello everyone,
I'm working on a project where I need to obtain samples from 4 ADC channels at 300KHz.

ARCHITECTURE
To achieve this, I'm utilizing the following peripherals:

PWM: This peripheral is responsible for triggering the entire sequence. The conversions defined in ADC_ETC are initiated through the VAL0 and VAL1 triggers. The period is set at 60us. I've been trying to lower the period, but doing so disrupts the functionality (Note: When I reduce the period, I also update the delays in the sequences defined in ADC_ETC).
LPADC1: This peripheral is where the conversions take place. In this case, two commands have been defined, one for reading channel A1_1 and another for reading channel A1_2. The total conversion time of each command is 256.25 ns.
LPADC2: Similar to LPADC1, this peripheral is used for conversions. Two commands have been defined here as well, one for reading channel A2_3 and another for reading channel A2_4.The total conversion time of each command is 256.25 ns.
ADC_ETC: This peripheral manages triggers. Four triggers have been defined:
DMA: Once all the conversions are completed, ADC_ETC0COCO0 is generated, initiating the transfer of the conversions. To retrieve all conversions, a transfer of 240 bytes is performed starting from address 0x40048010.
RESULTS
With this configuration, I'm able to perform readings correctly, but it appears that the operation is rather slow:

The period is set at 60us. Lowering the period disrupts the functionality (When I decrease the period, I also update the delays in the sequences defined in ADC_ETC). However, if I increase the period, it works correctly. This suggests that there might be some limitation affecting the system.
I would greatly appreciate any insights or suggestions on how to improve the performance.
iMXRT1170