A question about LTIB on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A question about LTIB on imx6q

Jump to solution
663 Views
paull
Contributor I

I have downloaded the BSP from the official website.And now I want to install LTIB on the UBUNTU14.04.According to the document I have install some libraries which the LTIB rely on.

sudo aptitude -y install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev

sudo aptitude -y install libdbus-glib-1-dev liborbit2-dev intltool

sudo aptitude -y install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool

sudo aptitude -y install uuid-dev liblzo2-dev

sudo aptitude -y install tcl dpkg

sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev

sudo apt-get install texinfo

And I have installed zlib1g & zlib1g-dev.According to the command:apt-cache policy,I am sure this two have been installed.After LTIB been installed ,some mistakes happen as follows when I run it:

defined(@array) is deprecated at /usr/local/arm/LTIB/ltib/bin/Ltibutils.pm line 362.

    (Maybe you should just omit the defined()?)

ltib cannot be run because one or more of the host packages needed to run it

are either missing or out of date or not in ltib's standard path.  Please

install/upgrade these packages on your host.  If you have your own utilities

in non-standard paths, please add an entry into the .ltibrc file for example:

%path_std

/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes

Package                Minimum ver   Installed info

-------                -----------   ---------------

zlib-devel             0             not installed

Died at ./ltib line 1409.

traceback:

main::host_checks:1409

  main:554

Started: Tue Jan 12 11:51:18 2016

Ended:   Tue Jan 12 11:51:18 2016

Elapsed: 0 seconds

Build Failed

At first there was another error like:zlib            0             not installed

So I found a file named "patch-ltib-ubuntu12.04.sh"and run it .Then this item disappeared.What should I do now?How can I install zlib-devel i need?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
512 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may just comment this line in "ltib" Perl script :

Package                Minimum ver   Installed info

-------                -----------   ---------------

#zlib                   0             not installed

  Also, please check environment setup, using "Setting_Up_LTIB_host.pdf"


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
513 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may just comment this line in "ltib" Perl script :

Package                Minimum ver   Installed info

-------                -----------   ---------------

#zlib                   0             not installed

  Also, please check environment setup, using "Setting_Up_LTIB_host.pdf"


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply