8MMINILPD4-EVK Hangs with clean Kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8MMINILPD4-EVK Hangs with clean Kernel

2,592 Views
lucas_tanure
Contributor I

Hi, 

I'm trying to build my own kernel to use with 8MMINILPD4-EVK, but the board doesn't boot.

Steps I'm using:

Set the board to download mode and flash  L4.14.98_2.0.0_ga_images_MX8MMEVK.zip

$ sudo ./uuu L4.14.98_2.0.0_ga_images_MX8MMEVK.zip

Build Kernel:

$ git clone https://source.codeaurora.org/external/imx/linux-imx
$ cd linux-imx
$ git checkout origin/imx_4.14.98_2.3.0 -b imx_4.14.98_2.3.0

$ export ARCH=arm64
$ export CROSS_COMPILE=aarch64-linux-gnu-
$ export PATH=/media/workspace/.bin/gcc-linaro-7.5.0-2019.12-x86_64_aarch64-linux-gnu/bin/:$PATH
$ make defconfig
$ make -j25 Image dtbs modules
$ make modules_install INSTALL_MOD_PATH=./modules

$ rm -rf ./modules/lib/modules/4.14.98-06659-g0347fe7527d06-dirty/build
$ rm -rf ./modules/lib/modules/4.14.98-06659-g0347fe7527d06-dirty/source

$ scp arch/arm64/boot/Image [email protected]:/run/media/mmcblk2p1/
$ scp arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dtb [email protected]:/run/media/mmcblk2p1/
$ scp -r ./modules/lib/modules/4.14.98-06659-g0347fe7527d06-dirty [email protected]:/lib/modules/

It a clean kernel, no changes made.

Kernel Hangs:
[ 0.994336] kvm [1]: 8-bit VMID
[ 0.997928] kvm [1]: GICv3: no GICV resource entry
[ 1.001977] kvm [1]: disabling GICv2 emulation
[ 1.006455] kvm [1]: GIC system register CPU interface enabled
[ 1.012367] kvm [1]: vgic interrupt IRQ1
[ 1.016315] kvm [1]: Hyp mode initialized successfully
[ 1.023633] audit: initializing netlink subsys (disabled)
[ 1.026926] audit: type=2000 audit(0.896:1): state=initialized audit_enabled=0 res=1
[ 1.027210] workingset: timestamp_bits=44 max_order=19 bucket_order=0
[ 1.046290] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.049831] NFS: Registering the id_resolver key type
[ 1.054399] Key type id_resolver registered
[ 1.058572] Key type id_legacy registered
[ 1.062608] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.069576] jffs2: version 2.2. (NAND) �� 2001-2006 Red Hat, Inc.
[ 1.075903] 9p: Installing v9fs 9p2000 file system support
[ 1.085214] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 1.089820] io scheduler noop registered
[ 1.093861] io scheduler cfq registered (default)
[ 1.098462] io scheduler mq-deadline registered
[ 1.103013] io scheduler kyber registered
[ 1.118988] imx-sdma 30bd0000.sdma: no iram assigned, using external mem
[ 1.124902] imx-sdma 30bd0000.sdma: Falling back to user helper
[ 1.130504] imx-sdma 302c0000.sdma: no iram assigned, using external mem
[ 1.139548] imx-sdma 302b0000.sdma: no iram assigned, using external mem
[ 1.152649] mxs-dma 33000000.dma-apbh: initialized  ## KERNEL HANGS

 

Tags (1)
0 Kudos
Reply
2 Replies

2,502 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

It may have some issues with this kernel release, since this release provides no statement of support or validation for anything except the target for this release.

 

If possible please try with L4.14.98-2.0.0 and check if the problem persist.

 

Thank you,

Best regards,

Aldo.

0 Kudos
Reply