8M Mini: Unused NAND_DQS Termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8M Mini: Unused NAND_DQS Termination

Jump to solution
782 Views
adevries
Contributor V

On the i.MX 8M Mini, I muxxed the NAND interface pins to act as the USDHC3 interface instead of a NAND interface. Does this mean I can leave NAND_DQS (ball R22) unconnected? Or does there still need to be a capacitor dummy load connected to the pin? I see that the evaluation board has a capacitor connected, but I'm not sure why.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
777 Views
igorpadykov
NXP Employee
NXP Employee

Hi adevries

 

yes in this case one can leave NAND_DQS unconnected.

 

Best regards
igor

View solution in original post

1 Reply
778 Views
igorpadykov
NXP Employee
NXP Employee

Hi adevries

 

yes in this case one can leave NAND_DQS unconnected.

 

Best regards
igor