I've recently tried the 3.0.35 kernel from L3.0.35_12.09.03_ER. It is very unstable no matter what kernel configuration I'm using, even on kernel provided in debian package in L3.0.35_12.09.03_ER
It crashes with errors like:
Unable to handle kernel paging request at virtual address ffffffff
pgd = ba2f4000
[ffffffff] *pgd=4fffe821, *pte=00000000, *ppte=00000000
Internal error: Oops: 17 [#1] PREEMPT SMP
Modules linked in:
CPU: 1 Not tainted (3.0.35 #1)
PC is at anon_vma_clone+0x4c/0x158
LR is at anon_vma_clone+0x3c/0x158
pc : [<800e0504>] lr : [<800e04f4>] psr: a00f0013
sp : bff8be78 ip : 0bfd7000 fp : 80ad8d40
r10: 00000000 r9 : ba142cf0 r8 : baa561c8
r7 : bff0e840 r6 : 00000000 r5 : ffffffff r4 : bfa31f78
r3 : bff8a000 r2 : 80a7fc90 r1 : 8003d004 r0 : bfa31f78
Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 4a2f404a DAC: 00000015
Process init (pid: 1, stack limit = 0xbff8a2f0)
Stack: (0xbff8be78 to 0xbff8c000)
be60: 2ab98fff bff0e878
be80: 80ad8d20 ba142cb8 bff0e840 ba142cb8 bff0e754 80acdd20 00000001 bff0e738
bea0: bc0b07dc 800e0630 bff0e840 bfc29040 ba142cb8 bff0e754 80acdd20 8007138c
bec0: bffd2054 00000020 bff0e744 bff0e758 bfc28000 bff8a000 bfc2803c bfc2907c
bee0: bc0178cc ba050000 01200011 80acdd20 bff8bf08 00000000 bff8bfb0 bff8a000
bf00: 7eabd718 80072118 bfd82c80 80a97fe0 ba0501d8 ba0501d0 bff8a000 00000000
bf20: 00000000 ba050124 00000020 00000000 bffd2000 01200011 00000000 2ab91360
bf40: 00000000 800416c4 bff8a000 00000000 2ad08000 80072534 2ab913c8 00000000
bf60: 00000000 bff8bf80 800416c4 7eabd91c 00000008 00000000 7eabd91c 80081910
bf80: 7ffbfeff fffffffe 00000000 00000000 0000000b 2ab913c8 7eabd720 2ab91360
<0>bfa0: 00000078 80041540 00000000 2ab913c8 01200011 00000000 00000000 00000000
bfc0: 2ab913c8 7eabd720 2ab91360 00000078 2ab91820 00000001 00000001 2ad08000
bfe0: 00000078 7eabd718 2ac97edf 2ac41276 000f0030 01200011 00000000 00000000
[<800e0504>] (anon_vma_clone+0x4c/0x158) from [<800e0630>] (anon_vma_fork+0x20/)
[<800e0630>] (anon_vma_fork+0x20/0x130) from [<8007138c>] (dup_mm+0x1a8/0x4d8)
[<8007138c>] (dup_mm+0x1a8/0x4d8) from [<80072118>] (copy_process+0x9e4/0xdb8)
[<80072118>] (copy_process+0x9e4/0xdb8) from [<80072534>] (do_fork+0x48/0x2a4)
[<80072534>] (do_fork+0x48/0x2a4) from [<80041540>] (ret_fast_syscall+0x0/0x30)
Code: e2504000 11a0a006 0a000024 e5985004 (e5956000)
---[ end trace 8479eb65fc3380dc ]---
Virtual addresses are different each time.
With kernel 3.0.15 and the same rootfs everything works perfectly. Have somebody experienced simillar issue?
Googling the issue suggests that the broken memory might be an issue, but I run the memcheck program on 3.0.15 kernel and it founds nothing.
I would really appreciate any help.
Regards,
Marcin Miklas
PS. More crashes attached.
Original Attachment has been moved to: 3.0.35_crashes.zip
已解决! 转到解答。
Daiane,
memtester is included in ubuntu repositories, if you try oneiric image then you can easily install it:
apt-get install memtester
You can also try play some video using gplay. It could make it crash faster.
Yes we have the same board revision.
I've took oneiric.tar.gz from L3.0.35_12.09.01_GA_images_MX6Q. Upgraded u-boot on the board to u-boot-mx6q-sabrelite.bin. Modified uboot environment a little to make it able read kernel from rootfs.
Problems are basically the same.
MX6Q SABRELITE U-Boot > printenv
bootdelay=3
baudrate=115200
ipaddr=192.168.1.103
serverip=_SERVER_IP_ADDR_
netmask=255.255.255.0
loadaddr=0x10800000
rd_loadaddr=0x11000000
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
bootargs=console=ttymxc1,115200
bootargs_base=setenv bootargs console=ttymxc1,115200
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
bootcmd_net=dhcp; run bootargs_base bootargs_nfs;bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
bootcmd=run bootcmd_mmc
clearenv=sf probe 1 && sf erase 0xc0000 0x2000 && echo restored environment to factory default
upgradeu=for disk in 0 1 ; do mmc dev ${disk} ;for fs in fat ext2 ; do ${fs}load mmc ${disk}:1 10008000 /6q_upgrade && source 10008000 ; done ; done
bootfile=_BOOT_FILE_PATH_IN_TFTP_
nfsroot=_ROOTFS_PATH_IN_NFS_
ethact=FEC0
bootcmd_mmc=for disk in 0 1 ; do mmc dev ${disk} ;for fs in fat ext2 ; do ${fs}load mmc ${disk}:1 10008000 /6q_bootscript && source 10008000 ;done ;done
stdin=serial
stdout=serial
stderr=serial
Environment size: 1171/8188 bytes
6q_bootscript contents:
set bootargs $bootargs root=/dev/mmcblk0p1 rootwait fixrtc ;
ext2load mmc ${disk}:1 10800000 /boot/uImage && bootm 10800000 ;
echo "Error loading kernel image"
In the U-Boot bootargs, the following doesn't seem correct:
video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
If the system is using dual-display, the second video needs to be on another framebuffer.
Jeff
"Error loading kernel image" is not an kernel error.
Your u-boot configuration are not good enough. Or, your kernel was not copied to right place.
Could you, please, use the default u-boot configurations and let me know the results?
And, could you, please, share how you copy uImage to your board?
(I thought you was getting a kernel crash)
The uboot config is good enough, it loads the kernel properly and runs it. The kernel gives the error:
"Unable to handle kernel paging request at virtual address 0004e844"
Also this uboot config runs 3.0.15 kernel properly.
I downloaded the 12.09 images, set up a uSD card just like yours and it loads and runs fine. I used the rootfs, not oneiric rootfs, but my uImage is stored on the uSD in /boot and loaded by 6q_bootscript.
You could try a little different setup, by burning the kernel to the uSD and use the "old" way to load it:
( Take care to use this command, make sure you get the correct device and not an internal hard drive )
( cat /proc/mounts will help you determine )
sudo dd if=rootfs/boot/uImage of=/dev/sdX seek=2k bs=512 && sync && sync
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x2000;bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
This method is not much different than what you are using though.
Do you have any devices connected to the Sabre Lite? I would recommend disconnecting everything except the power supply, uSD and console cable, see if that helps.
Thanks for checking this. I also tried rootfs.tar.bz2 from L3.0.35_12.09.01_GA_images_MX6Q. It crashed with the usual paging errors during touch screen calibration.
I'll also try with kernel written directly to sdcard, not partition. Maybe somehow it helps.
HannStar HSD100PXN1. Also dell keyboard is connected. But with keyboard disconnected everything behaves the same.
Also I'd like to say again, that this board works perfectly ok with 3.0.15 and 2.6.38 kernels.
Are you using the same uSD card for all three kernels? And the same rfs? It looks like it cannot load the init from the rfs properly. I know uboot loads the 6q_bootscript and uImage, but it seems it crashes where the rfs init starts after the kernel.
Maybe try a different card? Or try nfs mounted rfs? This is just a strange error, but maybe the 3.0.35 kernel is sensitive to the brand of uSD? ( That's why uboot reads it fine? ).
I'm using normal SD card, the same rootfs, I only change kernels. And sometimes with the 3.0.35 kernel everything starts up correctly (even my app is displaying) but after some playing with app it crashes with similar page error.
I tried many cards and even booting from TFTP. So that must be something else.