Hello,
I'm using 1Mbit CAN bus with i.MX7Dual.
1Mbit communication is not functional with SOC revision 1.3.
Problem description:
MX7D_PAD_I2C3_SCL__FLEXCAN2_RX 0x59
MX7D_PAD_I2C3_SDA__FLEXCAN2_TX 0x59
Is it a know issue?
Thanks,
Uri
Hi Uri
one can test flexcan with Demo Images from below link, also some additional info
was sent you via mail
can\test - imx-test - i.MX Driver Test Application Software
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I'm able to test the flexcan.
The problem is the rate of 1Mbit with i.MX7Dual rev 1.3.
Thanks,
Uri