1Mb CAN bus with i.MX7Dual rev 1.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1Mb CAN bus with i.MX7Dual rev 1.3

978 Views
urimashiach
Contributor III

Hello,

I'm using 1Mbit CAN bus with i.MX7Dual.

1Mbit communication is not functional with SOC revision 1.3.

Problem description:

  • Only the transmission  side is affected, listen only mode is functional.
  • Lower speeds are functional.
  • The problem is not detected with SOC revision 1.2.
  • Relevant pin-mux configuration:

            MX7D_PAD_I2C3_SCL__FLEXCAN2_RX        0x59
            MX7D_PAD_I2C3_SDA__FLEXCAN2_TX        0x59

Is it a know issue?

Thanks,

Uri

Labels (2)
0 Kudos
Reply
2 Replies

891 Views
igorpadykov
NXP Employee
NXP Employee

Hi Uri

one can test flexcan with Demo Images from below link, also some additional info

was sent you via mail

i.MX Software | NXP 

can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

891 Views
urimashiach
Contributor III

Hi Igor,

I'm able to test the flexcan.

The problem is the rate of 1Mbit with i.MX7Dual rev 1.3.

Thanks,

Uri

0 Kudos
Reply