請問i.MX283: 1.是不是沒有support Ethernet MII interface. 2.SPI NOR Flash 是不是只能接SSP2 port? 3. 如果同時support NAND Flash and SPI NOR Flash, UART是不是只剩下3 port可以用?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

請問i.MX283: 1.是不是沒有support Ethernet MII interface. 2.SPI NOR Flash 是不是只能接SSP2 port? 3. 如果同時support NAND Flash and SPI NOR Flash, UART是不是只剩下3 port可以用?

645件の閲覧回数
oa
Contributor I

請問i.MX283: 1.是不是沒有support Ethernet MII interface. 2.SPI NOR Flash 是不是只能接SSP2 port? 3. 如果同時support NAND Flash and SPI NOR Flash, UART是不是只剩下3 port可以用?

0 件の賞賛
4 返答(返信)

571件の閲覧回数
oa
Contributor I

ok, thanks.

0 件の賞賛

571件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi OA

i.MX283 supports NAND,SPI-NOR,UART,Ethernet connections and

its specific differencies can be found in

IMX28CEC  Table 2. i.MX28 Functional Differences

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

571件の閲覧回数
oa
Contributor I

Hi igor,

refer to IMX28CEC.PDF Page65, 4.5 i.MX283 Ball Map; some of MII function of i.MX283 are NC pin, could you help how to connection for Ethernet MII function?

2015-03-24_093238.bmp


0 件の賞賛

571件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi OA

you are right: ENET0_TXD2,3 ENET0_RXD2,3 are not

available on i.MX283. So seems MII is not possible with i.MX283.

~igor

0 件の賞賛