怎么将1080p的屏在linux下显示720p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

怎么将1080p的屏在linux下显示720p

3,300 Views
fulinux
Contributor IV

硬件平台:imx6q

软件平台:linux-3.0.35, Qt5.4

大家好,

我们现在遇到一个棘手的问题,想请nxp的同事帮我看看。我们现在是基于imx6q的平台做Qt程序应用,我们的屏是1920x1080@60, 使用了两路lvds(split mode), 我们用Qt5.4开放了一个小游戏,但是因为是一个1080p的屏所以帧率很低,很难满足要求。我们讨论将分辨率降下来用720p的分辨率显示,这个方案可以吗?如果可以有没有是吗文档可以参考一下,需要改哪里呢?我是一个新手,希望有个例子可以参考。

期待你们的回复!

谢谢!

fulinux.

Labels (2)
Tags (1)
0 Kudos
7 Replies

2,760 Views
joanxie
NXP TechSupport
NXP TechSupport

one can set uboot paramter to get 720p, for detailed information, I send uboot document and linux release note (table 11)to you for reference.

0 Kudos

2,760 Views
fulinux
Contributor IV

Hi joan,

   Are you still here, can you give me some advice about how to change resolution in linux of running(linux运行着的时候)?

0 Kudos

2,760 Views
joanxie
NXP TechSupport
NXP TechSupport

my understanding is that you want to support dual 1080p display, and video resolution is 720p,right?

if yes, they are belong to different hardware, imx6 IPU couldn't support dual 1080p@60 display,  but vpu can support 720p@30 video.

0 Kudos

2,759 Views
fulinux
Contributor IV

Hi joan,

    我们定制的开发板已经可以支持1080p屏,是用了双路lvds。问题是我们运行Qt的游戏程序时,游戏不流畅,帧率上不去,这个如何解决呢? 我的想法是进入游戏是能不能把分辨率降到720p?退出游戏的时候又恢复原来的1080p的显示?不知道你有没有明白我的意思?

智能钢琴 克洛斯威智能钢琴 

这个是我们的产品,是基于你们的平台,linux+Qt开发的,希望你们能提供帮助。

0 Kudos

2,759 Views
joanxie
NXP TechSupport
NXP TechSupport

do you use QtWayland to run the application instead of using X11 or EGLFS, right?  if yes, maybe you can refer to the link as below:

https://community.nxp.com/thread/333193 

0 Kudos

2,760 Views
fulinux
Contributor IV

Hi Joan,

  I have build a wayland rootfs, and copy a example of qtwayland to my board, it has some problem as following:

 ./qml-compositor
This application failed to start because it could not find or load the Qt platform plugin "xcb".

Available platform plugins are: eglfs, minimal, minimalegl, offscreen, wayland-egl, wayland.

Reinstalling the application may fix this problem.
Aborted

what's wrong? what should i do? (weston runs well).

0 Kudos

2,760 Views
fulinux
Contributor IV

Hi joan,

   but i just want to set 720p when i luanched a game,  and resume to 1080p when i exited a game. it doesn't always 1080p or 720p.

thanks!

0 Kudos