Hi jingyang xie,
After modifying the code, you need to locate the linux kernel directory(.../linux-imx/.../git/) in the terminal, and use the command "make".
All the best
Jian Jiang
Thanks for all,I have got it!
Hi jingyang xie,
You may need the command below to set the cross compile and architecture before execute the command "make"
export CROSS_COMPILE=~/<your path>/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-
export ARCH=arm
All the best
Jian Jiang
Hi jingyang xie,
After modifying the code, you need to locate the linux kernel directory(.../linux-imx/.../git/) in the terminal, and use the command "make".
All the best
Jian Jiang
Hi jingyang xie,
You need to download the source code first, and then modify the kernel code. Then build the source code. Here could you tell me which board and which version BSP are you using?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi DanWang,
the BSP is 4.15.1.2.0,the custom board is based on i.mx 6 solo x sabresd