大家好,
目前使用的芯片为imx6solo,使用的BSP为Yocto L4.1.15-2.1.0版本。
目前使用这个版本的BSP编译出来的QT版本为5.6,请问是否可以通过修改Yocto配置文件,生成QT5.5的版本。
目前暂不想通过升级整个Yocto版本,基于当前Yocto版本修改。
谢谢。
maybe you can try to build qt5.5 to replace it, you need porting by yourself, I send the links for reference
Building Qt5 using yocto on Wandboard - Wandboard Wiki
https://forum.qt.io/topic/52546/tuto-build-qt-to-cross-compile-for-arm
Hi Joan,
这个帖子Building Qt5 using yocto on Wandboard - Wandboard Wiki提到在yocto/build/conf/bblayers.conf文件增加meta-qt5配置。
我仔细查看了下我的yocto BSP中的bblayers.conf文件,里面已经包含了meta-qt5。
另外,这两个帖子的内容与我的问题不太一致。我的yocto BSP中已经配置了meta-qt5,并且qt的版本为5.6.1。我的问题是如何修改将qt从5.6.1版本修改为5.5.1,谢谢支持。
you can build a similar layer like qt5.6, don't need to remove qt 5.6,