你好:
我们现在使用的有两款片子,一款是sabresd6q,一款是sabresd6dl。他们使用的外围硬件都是一样的,包括内存、mmc等等。差别就是cpu不同。
在我们现在的平台上,生成sabresd6q的firmware,进行下载是能够正常下载的。
但是生成的sabresd6dl的firmware,进行下载,却不行,一直停留在jump osimage 。
我们使用的是32位的,2g的内存。
编firmware的流程如下:
1、在mx6dl_sabresd_mfg.h文件中,将
#define PHYS_SDRAM_1_SIZE (1u * 1024 * 1024 * 1024)
修改成了
#define PHYS_SDRAM_1_SIZE (1u * 2048 * 1024 * 1024)
2、在flash_header.S文件中,将参数替换成 生成的针对与dl的32位2g的内存参数。
3、
cd ~/myandroid/bootable/bootloader/uboot-imx
make distclean
make mx6dl_sabresd_mfg_config
make
4、将生成的u-boot.bin拷贝到从官网上新下的针对mx6dl系列的mfg-tool中的os irmware中,并修改名字为u-boot-mx6dl-sabresd.bin
请问这个步骤是否正确,是否还有那些地方需要更改。
修改了一下flash_header.S里面的参数后,能够出打印信息了,但是到了print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal 后,板子就断电,无法继续下载了。具体打印信息如下:
CPU: Freescale i.MX6 family TO1.2 at 792 MHz | ||
Thermal sensor with ratio = 182 | ||
Temperature: 41 C, calibration data 0x57f4c57d | ||
mx6q pll1: 792MHz | ||
mx6q pll2: 528MHz | ||
mx6q pll3: 480MHz | ||
mx6q pll8: 50MHz | ||
ipg clock | : 66000000Hz | |
ipg per clock : 66000000Hz | ||
uart clock | : 80000000Hz | |
cspi clock | : 60000000Hz | |
ahb clock | : 132000000Hz | |
axi clock : 198000000Hz | ||
emi_slow clock: 99000000Hz | ||
ddr clock | : 396000000Hz | |
usdhc1 clock : 198000000Hz | ||
usdhc2 clock : 198000000Hz | ||
usdhc3 clock : 198000000Hz | ||
usdhc4 clock : 198000000Hz | ||
nfc clock | : 24000000Hz | |
Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61012 [POR ] | ||
Boot Device: SPI NOR | ||
I2C: ready | ||
DRAM: 2 GB | ||
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3 | ||
Using default environment | ||
In: | serial | |
Out: serial | ||
Err: serial | ||
i2c_addr:chip address cycle fail(a1) | ||
i2c_addr failed | ||
Rad licell error!e | ||
Net: got MAC address from IIM: 00:00:00:00:00:00 | ||
FEC0 [PRIME] | ||
Hit any key to stop autoboot: 0 | ||
## Booting kernel from Legacy Image at 10800000 ... | ||
Image Name: Linux-3.0.35-2666-gbdde708 | ||
Image Type: ARM Linux Kernel Image (uncompressed) | ||
Data Size: | 3164384 Bytes = 3 MB | |
Load Address: 10008000 | ||
Entry Point: 10008000 | ||
Verifying Checksum ... OK | ||
## Loading init Ramdisk from Legacy Image at 10c00000 ... | ||
Image Name: uboot initramfs rootfs | ||
Image Type: ARM Linux RAMDisk Image (gzip compressed) | ||
Data Size: | 4545326 Bytes = 4.3 MB | |
Load Address: 00000000 | ||
Entry Point: 00000000 | ||
Verifying Checksum ... OK | ||
Loading Kernel Image ... OK | ||
OK | ||
Starting kernel ... | ||
Uncompressing Linux... done, booting the kernel. |
Linux version 3.0.35-2666-gbdde708 (rob@rob-All-Serious) (gcc version 4.6.2 2011
0630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20)
) #2 SMP PREEMPT Mon Sep 22 15:22:34 CST 2014 | |
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d | |
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache | |
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board | |
Memory policy: ECC disabled, Data cache writealloc | |
CPU identified as i.MX6DL/SOLO, silicon rev 1.2 | |
PERCPU: Embedded 7 pages/cpu @8c80e000 s5184 r8192 d15296 u32768 | |
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520192 |
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes) | |||
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes) | |||
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes) | |||
Memory: 2048MB = 2048MB total | |||
Memory: 2068348k/2068348k available, 28804k reserved, 360448K highmem | |||
Virtual kernel memory layout: | |||
vector : 0xffff0000 - 0xffff1000 ( 4 kB) | |||
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) | |||
DMA | : 0xf4600000 - 0xffe00000 ( 184 MB) | ||
vmalloc : 0xea800000 - 0xf2000000 ( 120 MB) | |||
lowmem : 0x80000000 - 0xea000000 (1696 MB) | |||
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) | |||
modules : 0x7f000000 - 0x7fe00000 ( 14 MB) | |||
.init : 0x80008000 - 0x8003a000 ( 200 kB) | |||
.text : 0x8003a000 - 0x805ada5c (5583 kB) | |||
.data : 0x805ae000 - 0x805fc600 ( 314 kB) | |||
.bss : 0x805fc624 - 0x806275b4 ( 172 kB) | |||
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 | |||
Preemptible hierarchical RCU implementation. | |||
NR_IRQS:624 | |||
MXC GPIO hardware | |||
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms | |||
Set periph_clk's parent to pll2_pfd_400M! | |||
arm_max_freq=800MHz | |||
MXC_Early serial console at MMIO 0x2020000 (options '115200') | |||
bootconsole [ttymxc0] enabled | |||
Console: colour dummy device 80x30 | |||
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280) | |||
pid_max: default: 32768 minimum: 301 | |||
Mount-cache hash table entries: 512 | |||
CPU: Testing write buffer coherency: ok | |||
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available | |||
CPU1: Booted secondary processor | |||
Brought up 2 CPUs | |||
SMP: Total of 2 processors activated (3162.11 BogoMIPS). | |||
print_constraints: dummy: | |||
NET: Registered protocol family 16 | |||
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal | |||
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal | |||
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal | |||
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal | |||
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal |
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal