关于IMX6UL第二个USB接口在linux驱动的问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

关于IMX6UL第二个USB接口在linux驱动的问题

3,141件の閲覧回数
我爱下载
Contributor III

usb2作为host,其ID已经直接接地,VBUS悬空,设备采用外部供电方式。设备树中加载了usb2的驱动

   usbotg2: usb@02184200 {
    compatible = "fsl,imx6ul-usb", "fsl,imx27-usb";
    reg = <0x02184200 0x200>;
    interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
    clocks = <&clks IMX6UL_CLK_USBOH3>;
    fsl,usbphy = <&usbphy2>;
    fsl,usbmisc = <&usbmisc 1>;
                ahb-burst-config = <0x0>;
                tx-burst-size-dword = <0x10>;
                rx-burst-size-dword = <0x10>;
    status = "disabled";
   };

&usbotg2 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_usbotg2>;
 dr_mode = "host";
    disable-over-current;
 status = "okay";
};

现在的问题是,系统启动后,在/sys/bus/usb/devices 下只能看到


1-0:1.0@ usb1@

如果给外部设备开机,系统一直在提示下面的信息:

usb 1-1: new high-speed USB device number 119 using ci_hdrc

但是无法识别出设备来,如果usb1接上外部设备了,usb2上就识别出来了,这是怎么回事

ラベル(1)
2 返答(返信)

1,882件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello JiYong,

    USB VBUS couldn't be floated, it should be supplied 5V power. try it , please!


Have a great day,
TIC   weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,882件の閲覧回数
我爱下载
Contributor III

非常感谢您的回复,我测试后发现确实VBUS必须接入确定的高电平。

0 件の賞賛
返信