关于调整uart_debug调试口问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于调整uart_debug调试口问题

1,607 Views
328670383
Contributor I

你好,根据官方给的imx8m原理图参考,uart_debug的调试口有两个:uart1和uart2,uart1 对应于A53 核,uart2对应M4核,如下图所示。现在想将两个调试串口合并为一个,如:将M4调试换到uart1上,需要软件如何设置,硬件是否需要改动?

希望给解答一下,万分感谢。

0 Kudos
1 Reply

944 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Huajian,

 See below, please!

1. Hardware

Don't need to modify it.

2. software

(1)You need to modify software in linux BSP: u-boot & dts

    this is for A53.

(2)You need to modiy firmware for M4

At first download SDK for M4 of i.MX8MQ from : https://mcuxpresso.nxp.com/en/select, select i.MX8MQ EVK , then select other items according to guidance.

Open it's one of  demo apps, you will find UART2 is used for Console. so modify it to UART1.

Have a nice day!

NXP TIC weidong sun

0 Kudos