分析:
1 示波器测试LVDS_T0+/T0-,LVDS_T1+/T1-,LVDS_T2+/T2-,LVDS_T3+/T3- 数据信号无任何的波形,只有偏置直流电平,但测试LVDS_CLK+/CLK-信号幅度正常,频率65MHZ正常
2 软件分析LOG提示:timeout when waiting for flip irq,显示irq异常而返回。LOG见附件
(1) 软件加入:write /sys/module/galcore/parameters/gpu3DMinClock 3 待测试。
(2)看贵司论坛的补丁如下的修改是否适应改IC?修改也没什么效果 。
- imx6q_set_lpm(WAIT_UNCLOCKED);
+ //imx6q_set_lpm(WAIT_UNCLOCKED);
cpu_do_idle();
- imx6q_set_lpm(WAIT_CLOCKED);
+ //imx6q_set_lpm(WAIT_CLOCKED);
spin_unlock(&master_lock);
goto done;
(2 ) 看代码是ipu出了问题,ipu_pre_yres_is_small。查询网上有一些客户提出该问题给NXP,但没得到正面解决问题的补丁。如帖子(Re: mxc_sdc_fb fb.16: timeout when waiting for fli... - NXP Community)
max_lu
Contributor I
Hi,
Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.
Looking at the blog below, there were issues with handling them, but we couldn't find any relevant patches (https://source.codeaurora.org/external/imx/linux-imx)
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Looking at the blog below, there were issues with handling them, but we couldn't find any relevant patches (https://source.codeaurora.org/external/imx/linux-imx)
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
NXP's kernel https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Hi,
Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.
IC screen printed as MCIMX6U7CVM08AC 。Which model does this IC belong to in the following list?
BSP already has the following patches by default, but the problem still exists.
patch:(if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_2_0) {)
static inline bool cpu_is_imx6sl(void) { return __mxc_cpu_type == MXC_CPU_IMX6SL; }
static inline bool cpu_is_imx6dl(void) { return __mxc_cpu_type == MXC_CPU_IMX6DL; }
static inline bool cpu_is_imx6sx(void) { return __mxc_cpu_type == MXC_CPU_IMX6SX; }
static inline bool cpu_is_imx6ul(void) { return __mxc_cpu_type == MXC_CPU_IMX6UL; }
static inline bool cpu_is_imx6q(void) { return __mxc_cpu_type == MXC_CPU_IMX6Q; }
if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_2_0) {
clk[IMX6QDL_CLK_LDB_DI0_SEL] = imx_clk_mux_flags("ldb_di0_sel", base + 0x2c, 9, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);
clk[IMX6QDL_CLK_LDB_DI1_SEL] = imx_clk_mux_flags("ldb_di1_sel", base + 0x2c, 12, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);
} else {
/*
* The LDB_DI0/1_SEL muxes are registered read-only due to a hardware
* bug. Set the muxes to the requested values before registering the
* ldb_di_sel clocks.
*/
disable_anatop_clocks();
init_ldb_clks(np);
clk[IMX6QDL_CLK_LDB_DI0_SEL] = imx_clk_mux_ldb("ldb_di0_sel", base + 0x2c, 9, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels));
clk[IMX6QDL_CLK_LDB_DI1_SEL] = imx_clk_mux_ldb("ldb_di1_sel", base + 0x2c, 12, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels));
}