下载并安装imx6q的BSP后,在安装后的LTIB文件夹下的uboot是适合imx6q_SABRA的吗

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

下载并安装imx6q的BSP后,在安装后的LTIB文件夹下的uboot是适合imx6q_SABRA的吗

ソリューションへジャンプ
2,075件の閲覧回数
zhongnanshi
Contributor I

如题,在官网下载并安装了L3.0.35_4.1.0_SOURCE后安装,安装完成后出现LTIB/PKGS文件夹,在pakgs文件夹下的uboot_2009.08这个是原始的源代码还是已经修改过能启动官方的开发板IMX6Q_SABRA的代码。

谢谢

ラベル(1)
0 件の賞賛
返信
1 解決策
1,565件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Nan,

In our website there is a porting guide you can refer to .

Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,565件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi zhongnan,

The uboot_2009.08 in the ltib/rpm/BUILD is the u-boot source code. The i.mx6Qsabresd board u-boot code you can see is /ltib/rpm/BUILD/uboot_2009.08/board/freescale/mx6q_sabresd/mx6q_sabresd.c. When you finish build the source code the u-boot and kernel images u-boot.bin, uImage you can see them under the /ltib/rootfs/boot directory.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,565件の閲覧回数
zhongnanshi
Contributor I

hi  Dan

something error,because after i install BSP , only  linux&linux_3.0.35 in the ltib/rpm/BUILD, i will reinstall the BSP.

0 件の賞賛
返信
1,565件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi nan,

If you reinstall the BSP, you need to delete the ltib file and the /opt packages.

Have a great day,

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,565件の閲覧回数
zhongnanshi
Contributor I

您好

我看到了 uimage和 u-boot.bin,这个uboot2009_2008的源代码你们官方只修改了mx6q_sabresd.c部分吗,其他都没有修改吗,如果我的硬件有变动,秩序修改这个文件吧 

  谢谢

0 件の賞賛
返信
1,566件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Nan,

In our website there is a porting guide you can refer to .

Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,565件の閲覧回数
zhongnanshi
Contributor I

thank you Dan

i got it.

0 件の賞賛
返信