PXP hands on with IMXRT1070

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PXP hands on with IMXRT1070

PXP hands on with IMXRT1070

This hands on is based on the evkmimxrt1170_pxp_lab_cm7.zip which is from

https://community.nxp.com/t5/i-MX-RT1170-CAS-Training/PXP-Multiple-Files/ta-p/1178709

this hands on give an example to understand pxp basic concept like letterbox background color, rotation, ps buffer coordination definition, output buffer coordination definition more clear

 

  • No Roation

This test is based on no rotation, so define as below

#define LAB1_BIT_BLIT_NO_ROTATION

This demo output is that the rabbit picture shows on the upper left corner of lcd, and the offset width and height is 100

 

#ifdef LAB1_BIT_BLIT_NO_ROTATION

    PXP_ps_bitblit(

                   // input

                   (void*)bmp_rabbit,

                   PIXEL_BYTES,

                   BMP_RABBIT_WIDTH,

                   BMP_RABBIT_HEIGHT,

 

                   // output

                   s_BufferLcd[curLcdBufferIdx],

                   DEMO_PANEL_WIDTH,

                   DEMO_PANEL_HEIGHT,

                   100,  // output offset x

                   100,  // output offset y

                   kPXP_No_Rotate);

#endif

 

 

 

in this lab sample code, the background is set to black,

PXP_SetProcessSurfaceBackGroundColor(APP_PXP, 0U);

 

The output is

joanxie_0-1667802290435.png

 

 

If we want to set the background to lighter blue, this is what I want to get

joanxie_1-1667802290479.png

 

 

then I modify the code to

PXP_SetProcessSurfaceBackGroundColor(APP_PXP, 0xFFF0U);

 

But we get the same output like, without any difference

 

joanxie_2-1667802290515.png

 

 

 

Check the code, find that the original code

 

void PXP_ps_sub_region_bitblit(…)

{ …..

    outputBufferConfig.width = sub_region_width;

    outputBufferConfig.height = sub_region_height;

  ……

}

 

This means that the output buffer width and height are the same as the picture width and height, so whatever background color you set, you couldn’t find anything difference, then change the output buffer width and height is the same as lcd width and height

 

 

void PXP_ps_sub_region_bitblit(…)

{ …..

      outputBufferConfig.width = output_width;

      outputBufferConfig.height= output_height;

  ……

}

 

Then the output change to

joanxie_3-1667802290566.png

 

 

We can find the color on the top of display is still black and this isn’t what I need, still tracing the code

 

void PXP_ps_sub_region_bitblit(…)

{ …..

 // Output buffer

 outputBufferConfig.buffer0Addr   =  (uint32_t)output_buffer + output_offset_y * output_width * pic_bytes_per_pixel + output_offset_x * pic_bytes_per_pixel

……

}

 

output_buffer is defined as lcd buffer start address, here the output buffer start address isn’t defined as lcd buffer start address(output_buffer), this is offset of lcd buffer start address, so change it like

 

void PXP_ps_sub_region_bitblit(…)

{ …..

 // Output buffer

 outputBufferConfig.buffer0Addr = (uint32_t)output_buffer

……

}

 

Then the output is like

 

joanxie_4-1667802290623.png

 

 

The output picture move to the upper left corner without offset, but this demo defines the offset is 100

 

void PXP_ps_sub_region_bitblit(…)

{ …..

 // PS buffer

PXP_SetProcessSurfacePosition(APP_PXP,0,0,BMP_RABBIT_WIDTH - 1U,

BMP_RABBIT_HEIGHT - 1U);

…..

}

 

In the original code, the PS buffer offset is 0, because the ps buffer start address is the same as the output buffer start address, and output buffer start address is offset + lcd output buffer start address, so set the PS output offset is 0, but I change the output buffer start address is the same as lcd buffer start address, so change the code

 

void PXP_ps_sub_region_bitblit(…)

{ …..

            uint32_t psUlcX         = output_offset_x;

            uint32_t psUlcY         = output_offset_y;

            uint32_t psLrcX, psLrcY;

            psLrcX = psUlcX   +  sub_region_width  - 1U;

            psLrcY = psUlcY + sub_region_height- 1U;

        // PS buffer

        PXP_SetProcessSurfacePosition(APP_PXP,psUlcX,psUlcY,psLrcX,psLrcY);

…..

}

 

The output is

joanxie_5-1667802290673.png

 

\

 

Now this is what we need

 

 

  • Roation

Set Macro to #define LAB2_BIT_90_DEGREE_ROTATION

 

The output is

joanxie_6-1667802290728.png

 

 

When rotation is 90 degree and width is wider than the output height, the display part will be cut, so change the code from

Before

void PXP_ps_sub_region_bitblit(…)

{ …..

      outputBufferConfig.width = output_width;

      outputBufferConfig.height= output_height;

…..

}

 

To

 

void PXP_ps_sub_region_bitblit(…)

{ …..

 if  (rotate == kPXP_Rotate90)

 {

    outputBufferConfig.width          = output_height;        /*Joan*/

    outputBufferConfig.height         = output_width;         /*Joan*/

 }

else

{

        outputBufferConfig.width          = output_width;         /*Joan*/

        outputBufferConfig.height         = output_height;        /*Joan*/

}…..

}

 

Because this demo only shows no rotation and 90 degree rotation, if customer needs 270 degree, 180 degree, can add by themselves

附件
无评分
版本历史
最后更新:
‎11-06-2022 11:44 PM
更新人: