The i.MX 8QXP introduces a concept for manipulating resource allocation, power, clocking and IO configuration and muxing, the System Controller Unit (SCU) has been added to the system. The SCU is an Arm Cortex-M4 core and is the first processor to boot in the i.MX 8QXP design.
It is the responsibility of the SCU to control:
All those subsystems are abstracted thanks to the System Controller Firmware (SCFW) running in the SCU. Other software components communicate with SCU via an Application Programming Interface (API).
This API makes Remote Procedure Calls (RPC) via an underlying Inter-Processor Communication (IPC) mechanism. Each OS distributed by NXP features a library that allows it to interact with the SCFW running on the SCU.
The SCU sub-system is made out of:
It includes the following set of peripherals:
System Controller Firmware (SCFW)
NXP only releases packages in a majority object code form, however a board.c file is provided in which most of the configuration of the SCFW can be done.
The first main step from SCFW to configure the DDR and start all other cores in the system. The boot flow is described in the image below:
The i.MX8 boot sequence involves SCU ROM, SCFW, Security Controller (SECO) ROM, and SECO FW:
From this point SCFW takes over and loads any image to the Arm Cortex-M or Cortex-A cores.
Downloading and building SCFW
Download the Arm GCC toolchain from here:
https://developer.arm.com/open-source/gnu-toolchain/gnu-rm/downloads
Export the toolchain to compile SCFW:
mkdir ~/gcc_toolchain
cp ~/Downloads/gcc-arm-none-eabi-10.3-2021.10-linux.tar.bz2 ~/gcc_toolchain/
cd ~/gcc_toolchain/
tar -xvjf gcc-arm-none-eabi-10.3-2021.10-linux.tar.bz2
export TOOLS=~/gcc_toolchain/
Download the file IMX-SCFW-PORTING-KIT-1.4.2 from NXP.
After the SCFW porting kit is downloaded and un-tar, navigate into packages and run the binary file inside:
$ cd <download-dir>/packages/
$ chmod a+x imx-scfw-porting-kit-1.4.2.bin
$ ./imx-scfw-porting-kit-1.4.2.bin
Navigate inside the newly created “imx-scfw-porting-kit” and into “src”. Extract the desired SCFW porting kit.
$ cd imx-scfw-porting-kit-1.4.2/
$ tar -xvf src/scfw_export_mx8qx.tar.gz
$ cd scfw_export_mx8qx/
The tar file extracted will be different depending on which board is being used.
All the code that is specific to a board configuration is under “platform/board/mx8qxp_mek/board.c”
To compile SCFW type the following command:
$ make qx B=mek R=B0
All the files resulting from compilation can be found inside build_mx8qx/