Minicom is a terminal emulation that can access a remote serial console enabling the configuration of RedBoot or the flash file system of the board.
Reach the configuration by typing CTRL-A Z
Press key Z after releasing CTRL and A!
Configure Minicom to work with i.MX by following the procedures below.
At the screen configuration, type O, choosing cOnfigure Minicom
In menu, choose Serial Port Setup
Below, the configuration option:
+-----------------------------------------------------------------------+
| A - Serial Device : /dev/ttyS0 |
| B - Lockfile Location : /var/lock |
| C - Callin Program : |
| D - Callout Program : |
| E - Bps/Par/Bits : 115200 8N1 |
| F - Hardware Flow Control : No |
| G - Software Flow Control : No |
| |
| Change which setting? |
+-----------------------------------------------------------------------+
Type the letter of option to enable the modification.
Remember to choose the right Serial Device