vulkan without display server (Wayland,X11)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vulkan without display server (Wayland,X11)

4,760件の閲覧回数
PeterBergin
Contributor III

Hi,
I'm trying to run a Vulkan application and render directly to the display without using any Window Manager/Display Server. My SoC is i.Mx8M (nitrogen8M board from Boundary Devices). Does NXP support to render directly to the display as I'm trying to do? Any example anyone can provide?

To test if this works I have cross-compiled Vulkan-Samples with help of a SDK built with Yocto (dunfell branch).

$ source <sdk-path>/environment-setup-aarch64-fslc-linux
$ git clone https://github.com/KhronosGroup/Vulkan-Samples.git
$ cd Vulkan-Samples && mkdir armbuild && cd armbuild
$ cmake -DVKB_DIRECT_2_DISPLAY=true ..
$ make -j4
$ scp app/bin/Release/aarch64/vulkan_samples <to-target>:

On target:
$ ./vulkan_samples --test hello_triangle

[info] Logger initialized
[info] Window created
[info] Initializing vulkan instance.
[info] Enabled Validation Layers:
[info] Found GPU: VeriSilicon
[warning] Couldn't find a discrete physical device, picking default GPU
[info] Initializing vulkan device.
[info] format_count 1 formats[0].format 44
[er[13733.152366] 002: audit: type=1701 audit(1599040557.574:11): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=310 comm
="vulkan_samples" exe="/home/root/vulkan_samples" sig=6 res=1
ror] [samples/api/hello_triangle/hello_triangle.cpp:535] Detected Vulkan error: ERROR_OUT_OF_DATE_KHR
Aborted

The example bails out here: https://github.com/KhronosGroup/Vulkan-Samples/blob/fb6bab484199c9406ba1b2ffbadb91971c519b14/samples... with the error code ERROR_OUT_OF_DATE_KHR.

Package versions:

libvulkan1-1.2.135.0-r0.aarch64.rpm
libvulkan-imx-6.4.0.p2.0+aarch64-r0.aarch64_mx8m.rpm
kernel-module-imx-gpu-viv-6.4.0.p2.4+fslc+git0+f2e8483fbd-r0.nitrogen8m.rpm
kernel-5.4.50-rt32+gde0fe9b79719-5.4.50+git0+503a3dce96-r0.nitrogen8m.rpm (linux-boundary)

I hope I can get some hints to get forward and information if the use case I'm trying is something that shall be possible on i.Mx8M.

Thanks,
/Peter

0 件の賞賛
返信
5 返答(返信)

4,511件の閲覧回数
KailoKyra
Contributor II

I'm having the same issue with that "AXI BUS ERROR" when trying to do render to the display directly without using Wayland and the Wayland surface extension.

Have you eventually found a solution to this issue ?

I'm trying not to use /dev/fb0 here, but to do it in a "direct-to-display" way without having to map or use the kernel's own framebuffer, and configuring the connector / display / mode and such myself.

0 件の賞賛
返信

4,719件の閲覧回数
PeterBergin
Contributor III

One step ahead...

To be able to create a swapchain the kernel config option CONFIG_DRM_FBDEV_OVERALLOC must be set to something greater than 100, which is default. This in order for libvulkan to be able to allocate bigger buffer than the screen from /dev/fb0. When I have set CONFIG_DRM_FBDEV_OVERALLOC I have passed the swapchain allocation in the example application.

But then I hit the next thing. A crash somewhere in the GPU code and a frozen system.

[ 269.477226] AXI BUS ERROR
[ 269.477245] GPU[0](ChipModel=0x7000 ChipRevision=0x6214):
** 439 printk messages dropped **

So, my question still remains, does libvulkan_VSI.so support rendering directly to /dev/fb0?

/Peter

0 件の賞賛
返信

4,757件の閲覧回数
PeterBergin
Contributor III

Adding output from vulkaninfo for more details.

0 件の賞賛
返信

4,735件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Peter,

 

The example works with latest BSP L5.4.24 on the EVK with wayland, You might try to get it.

 

Regards

 

0 件の賞賛
返信

4,733件の閲覧回数
PeterBergin
Contributor III

@Bio_TICFSL - does the example work to render directly to /dev/fb0? Or are you saying that the example is working when you use wayland and render to a wayland display?

0 件の賞賛
返信