imx8qxp sc16is750 ==> I can't see ttySC0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp sc16is750 ==> I can't see ttySC0

2,111 Views
yoonseok
Contributor III
Hello, I'm asking for help because I have a problem.


From imx8qxp chip, use sc16is750
I want to implement i2c to uart.


The following was added to file imx8x-mek-rpmsg.dtsi.

sc16is750: sc16is750@4d {
        compatible = "nxp,sc16is750";
        reg = <0x4d>;
        clocks = <&sc16is750_clk>;
        interrupt-parent = <&lsio_gpio1>;
         interrupts = <2 IRQ_TYPE_EDGE_FALLING>;
        gpio-controller;
        #gpio-cells = <2>;
       
        sc16is750_clk: sc16is750_clk {
                       compatible = "fixed-clock";
                      #clock-cells = <0>;
                      clock-frequency = <7372800>;
           };
};

When the system boots, the following message appears.
serial serial0: tty port ttySC0 registered

After the system boot,
ttySC0 is not visible in the /dev directory.

For reference, the gpio function added to sc16is750 operates normally.

What's the problem? Please help me.
0 Kudos
2 Replies

2,108 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yoonseok

 

for this case may be recommended to check if i2c is not owned by m4 resource, as in below

example (i2c1)

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek-rp...

In such case one can move i2c resource to A core as in below example sect."Modifying default configuration" (moving FlexCAN resources from the M4 partition to the A cores partition)

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-...

Or try to use dts without "rpmsg", not use m4 core.

 

Best regards
igor

0 Kudos

2,097 Views
yoonseok
Contributor III

It was solved thanks to you.Thank you.

0 Kudos