HellO
I created an RTSP OS Image
References URI
https://www.hackster.io/flint-weller/a-first-yocto-build-for-the-nxp-i-mx-8m-quad-evk-02b6a9
I doing pahse
1.Enable the layer meta-openembedded/meta-multimedia:
Add the line BBLAYERS += "${BSPDIR}/sources/meta-openembedded/meta-multimedia" to the configuration file
$yocto_root/build/conf/bblayers.conf.
2. Include gst-rtsp-server into the image build:
Add the line IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" to the configuration file $yocto_root/build/
conf/local.conf.
3. Run bitbake for your image to build with gst-rstp-server.
bitbake imx-image-multimedia
ERROR ) 4.I can't find the test-uri binary in the folder:
$yocto_root/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/
$version/
build/examples/
There is no cortexa9hf-vfp-neon-poky-gnueabi folder
build/tmp/work/
Also
Is it possible to use Python Pakage?
Spoilerfrom gi.repository import GstRtspServer