Eiq software has the problem of slow training speed during training and low CPU utilization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eiq software has the problem of slow training speed during training and low CPU utilization

3,083 Views
shaenhurst
Contributor I

When I was training the model, the training speed was very slow, the input image size was 160*160, and the batch size was 32. Normally, the time of each step will not exceed 1 second, and in the training of the previous period of training, the training time of each step is indeed no more than 1 second. But today when training is very slow, the training time per step has reached about 3 seconds without the same parameters. But the GPU usage rate and video memory occupancy rate remain normal, and I don't know how to solve it.

CPU model: i5 10210u

graphics card model: mx250

Memory size: 16g

Graphics card memory size:4g

0 Kudos
1 Reply

2,955 Views
david_piskula
NXP Employee
NXP Employee

Hello @shaenhurst,

can you provide more information about the dataset so that we can attempt to reproduce your issue on our side and analyze it? Are you using a publicly available dataset?

Thanks,

David

0 Kudos