wlan 8897 Wakeup card timeout issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wlan 8897 Wakeup card timeout issue

3,241件の閲覧回数
PeterYang_TW
Contributor I

Hello NXP Team,

We use Synaptics chip as a host and our Wi-Fi chip is 8897.
If our system entered standby, we found Wi-Fi and BT can't work after some hours.

We got the following errors:
[40901.633724] Wakeup device...
[40902.573041] CPU3: update max cpu_capacity 853
[40902.670385] logd: logdr: UID=1000 GID=1000 PID=1216 n tail=0 logMask=4 pid=0 start=0ns timeout=0ns
[40903.762661] wlan0:
[40903.762669] QUEUE_CMD: cmd=0xd1 is queued
[40904.701838] logd: logdr: UID=1000 GID=1000 PID=1216 n tail=0 logMask=4 pid=0 start=0ns timeout=0ns
[40904.713041] wlan_wakeup_card_timeout_func: ps_state=3
[40904.713046] Wakeup card timeout!
[40904.713052] event id:0x80000012
[40904.713061] Driver version = SD8897-15.68.19.p59-C3X15C698-GPL-(FP68)
[40904.713063] main_state = 4
[40904.713065] ioctl_pending = 1
[40904.713067] tx_pending = 4

We can reproduce this issue on SD8897-15.68.19.p59.1-C3X15CS698.p1-GPL-(FP68) and SD8897-15.68.19.p18-C3X15C612-GPL-(FP68).

Please help us provide a patch to fix this issue.

Attached is the log file and this message(wlan_wakeup_card_timeout_func) is at line 80523. 

BR,
Peter 

ラベル(2)
0 件の賞賛
14 返答(返信)

3,195件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @PeterYang_TW ,

 

Try the command of loading driver:

insmod sd8897.ko driver host_mlme=1 drvdbg=0x6 cfg80211_wext=0xf sta_name=wlan wfd_name=p2p max_vir_bss=1 ps_mode=1 auto_ds=1 drv_mode=7 p2p_enh=1 wakelock_timeout=30  cal_data_cfg=cal_data.conf 

 

Regards,

weidong

0 件の賞賛

3,190件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun,

What are ps_mode=1 and auto_ds=1?
Could you list all the values and its meaning for ps_mode and auto_ds?

We will try this command that you provided.

Thanks.
Peter

0 件の賞賛

3,176件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

ps_mode=1, 802.11 power saving mode is supported.

ps_mode=2, 802.11 power saving mode is disabled.

auto_ds=1, chip will automatically enter deep sleep mode.

audo_ds=2, automaical deep sleep function is disable.

 

So 

ps_mode=1 & auto_ds=1 means the chip supports power saving mode.

ps_mode=2 & auto_ds=2 means the chip will not enter into power saving mode.

 

Regards,

weidong

 

0 件の賞賛

3,171件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun,

Thank you for the information.

I have another question.
If we didn't set ps_mode and auto_ds, what's the default setting after loading driver?
We want to find the root cause of this issue.

BR,
Peter

0 件の賞賛

3,155件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun,

This issue can be reproduced with ps_mode=1 auto_ds=1.
Attached is the test log. Could you help us analyze the log to find the root cause?

BR,
Peter

0 件の賞賛

3,145件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

Please set ps_mode=2 auto_ds=2 !

Then try it. and tell me result, please!

 

Regards,

weidong

0 件の賞賛

3,141件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun,

We tested with ps_mode=2 auto_ds=2 and WiFi still works fine after 50 hours.

I referred to this discussion https://community.nxp.com/t5/Wireless-Connectivity/SD9098-quot-abnormal-driver-state-quot/m-p/149581... to set ps_mode=2 and auto_ds=2 when loading driver. 

We still want to know the root cause.

Thanks,
Peter

0 件の賞賛

3,133件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

When setting ps_mode=1 & auto_ds=1 , chip will automatically enter into power savming mode, and AP's beacon frame will wake it up.

If your host does not have a hardware wake-up mechanism to connect to WIFI, when your host wakes up, the wifi is still in sleep.
For example:
If there is a GPIO on the host side connected to WIFI (wake-up pin), when the host wakes up, it will also wake up the wifi.

 

Regards,

weidong

0 件の賞賛

3,124件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun,

Thank you for your information.

These two pictures are our wifi electrical diagram. Our host has a hardware wake-up mechanism to connect to WIFI. When the "Wakeup card timeout" occurred, our host was still on standby.
The root cause doesn't look like "when your host wakes up, the wifi is still in sleep."

PeterYang_TW_0-1679016781115.png

PeterYang_TW_2-1679017119316.png

BR,
Peter

0 件の賞賛

3,107件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

I sent email to you.  check it, please!

I was a little confused, so we discuss it in email directly.

 

Regards,

weidong

0 件の賞賛

2,948件の閲覧回数
PeterYang_TW
Contributor I

Dear @weidong_sun ,

Do you have any updates about this issue?

BR,
Peter

0 件の賞賛

2,939件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

I have ever sent email to you, did you receive it?

 

Regards,

weidong

0 件の賞賛

3,205件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

Could you help to provide some information I need?

1. Linux kernel version.

2. detailed operation steps, including loading driver.

Note:

This is the latest driver for 8897 , could you try it?

weidong_sun_0-1678876315711.png

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-...

 

Regards,

weidong

0 件の賞賛

3,201件の閲覧回数
PeterYang_TW
Contributor I

Hi @weidong_sun 

Please refer to my following reply.

1. Linux kernel version.
Our Linux version is 4.9.96

2. detailed operation steps, including loading driver.
loading driver -
insmod 8897mlan.ko
insmod sd8897.ko driver host_mlme=1 drvdbg=0x6 cfg80211_wext=0xf sta_name=wlan wfd_name=p2p max_vir_bss=1 drv_mode=7 p2p_enh=1 wakelock_timeout=30  cal_data_cfg=cal_data.conf
insmod mbt8897.ko

operation steps -
1. Connect to 2.4 or 5 GHz AP
2. Connect to BT RCU
3. Press a power key and our android box entered standby. 

This issue can be reproduced with the latest driver SD8897-15.68.19.p59.1-C3X15CS698.p1-GPL-(FP68).

BR,
Peter

0 件の賞賛