Hi
We are using the MicroMac (mmac.h) and our init is this:
How do we set the Transmit Power Level and the High Power mode for the M05 module?
In a non-MMAC way we'd use these:
Can they be done together with MMAC or are there other functions to use?
Thanks
ok, I've seen this post:
It indicates these functions exist:
To set just the power level the vMiniMac_PLME_SetReq_Power() function should be used the parameter is the same format as for eAppApiPlmeSet() described in JN-UG-3024 IEEE 802.15.4 Stack User Guide available from IEEE 802.15.4|JN516x MCUs|NXP
But you will only need to do this to lower the power as the default is to use full power.
They may also need to configure for a high power module for this vMiniMac_SetHighPowerMode() can be used this uses the same parameters as vAppApiSetHighPowerMode() also described in JN-UG-3024.
But in the latest SDK (JN-SW-4163) I cannot find these in any header file. (Build Number 1416)
Is there a newer SDK build somewhere or is this in a different SDK
Hello,
Could you please help me check this other thread?
https://community.nxp.com/thread/515065
I believe the document in the post should help you.
Regards