kw36/kw38 flash usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kw36/kw38 flash usage

1,642件の閲覧回数
frank-li2021
Contributor III

what's the flash/ram usage, about lib_ble_5-0_host_cm0p_gcc.a and lib_ble_kw36z_controller_gcc.a

I need do a evaluation for the chip

is there some doc for reference, about the usage?

タグ(1)
0 件の賞賛
6 返答(返信)

1,598件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @frank-li2021,

 

I hope you are doing great.

Please look at the release notes that we provide on the SDK.

"\SDK_2_2_9_FRDM-KW36\docs\MCUXpresso SDK Release Notes_MKW36Z4.pdf" for example.

It also will depend on the example that you are working on, and the role that you want.

Regards,

Mario

 

0 件の賞賛

1,570件の閲覧回数
frank-li2021
Contributor III

thant you for your reply

but I don't find the docs, while I'm creating the project with mcuXpresso IDE

there're only some docs about freertos under the doc folder

please attach the link of releaes note, I'll check the flash/ram usage in it

 

0 件の賞賛

1,557件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @frank-li2021,

Please look at the next image, the doc folder is could be download it.

mario_castaneda_0-1633703842727.png

Regards,

Mario

0 件の賞賛

1,547件の閲覧回数
frank-li2021
Contributor III

thank you so much

1,635件の閲覧回数
frank-li2021
Contributor III

 @nxf56274 

Hi Da Li

目前有资料说明 BLE lib 和 controller LIB 占多少 flash 和 ram 空间吗

我编译了一个  shell 的 demo ,从 map 文件分析,这两个库占了160+ 的 flash,这个数据对吗

或者有其他 资料可以参考,请帮忙 share 下 多谢

0 件の賞賛

1,634件の閲覧回数
frank-li2021
Contributor III

frankli2021_0-1632985849565.png

 

0 件の賞賛