hi someone,
will the FlexRAM could be configured as general RAM at KW36 platform?
there is no demo code nor help doc about this issue.
Regards,
Hi,
Hope you are doing well. Yes, the FlexRAM can be used as a traditional RAM.
From the Reference Manual (Chapter 29):
Could you please check section 29.4.11.17?
The Set FlexRAM Function command changes the function of the FlexRAM.
Hope this helps.
Best Regards,
Ricardo