Zigbee packet sniffing with FRDM-KW41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee packet sniffing with FRDM-KW41Z

1,626 Views
apnagy
Contributor I

I was curious about creating a zigbee packet sniffer using the FRDM-KW41Z devkit and Wireshark. 

Is there an easy way to do this?

Do I require the USB dongle to be able to sniff zigbee packets? 

Labels (3)
Tags (1)
0 Kudos
3 Replies

1,360 Views
ovidiu_usturoi
NXP Employee
NXP Employee

Hi apnagy@silabs.com‌,

Please see some details in the following topic USB-KW41 BLE Sniffer Application Update 

Let us know if you need more details,

Regards,

Ovidiu

0 Kudos

1,360 Views
apnagy
Contributor I

Thanks for the reply Ovidiu, 

I've tried that guide and experienced the following:

FRDM-KW41Z plugged into a USB port. 

I've flashed the mentioned firmware "KW41_802.15.4_SnifferOnUSB.bin" to the device.

After which the device LED4 lights up. 

At this point I've tried the Protocol Analyzer Adapter and the Protocol Analyzer panel in the NXP Test Tool. 

But neither can detect my connected KW41Z. 

Is there an other firmware I need to flash for the FRDM-KW41Z?

Regards,

Árpád

0 Kudos

772 Views
BasWep
Contributor I

Hello,

Is it possible to use FRDM-KW41Z as sniffer or only the USB-KW41?

Grtz

Bas

0 Kudos