Zigbee: I do not see any description of ZPS_tsNwkNib structure related to the Network Layer Information Base (NIB) in the application C code provided with JN-AN-1221. Could you please help?. Also in the AgeChildren.c file there are constants like ZPS_NWK_NT_AP_RELATIONSHIP_CHILD and ZPS_NWK_NT_AP_DEVICE_TYPE_ZED. Where are they defined?
The constants ZPS_NWK_NT_AP_RELATIONSHIP_CHILD and ZPS_NWK_NT_AP_DEVICE_TYPE_ZED are defined in a file named zps_nwk_nib.h which is located in the C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Components\ZPSNWK\Include folder.