I am trying to run the coordinator from JN-AN-1217-Zigbee-3-0-Base-Device on JN5169. But the device seems to be stuck at ZPS_eAplAfInit(). Found this by inserting some debug printout, it seems like ZPS_eAplAfInit does not return. Any idea why?
***********************************************
* COORDINATOR RESET *
***********************************************
APP: Entering APP_vSetUpHardware()
APP: Entering APP_vInitResources()
APP: Entering APP_vInitialise()
Initialising UART ...DoneAPP: Watchdog timer has reset device!
Hi Jia Jun Tan,
I am running into a similar issue, what did you do to resolve this issue?
Are you using a custom board or the eval kit ?
I am using a custom board.
My issue is similar in that I also use a JN5169 chip and that my code gets stuck in ZPS_eAplAfInit().
But it is different in that I use a modified JN-AN-1223 (v1008 with added CIE code from JN-AN-1201) with JN-SW-4168 (v1470)
I had it previously working in an older version of JN-SW-4168, but wanted to update the SDK for some newer functions and bug fixes.
So I thought the OP might have some advice on how to get past the code being stuck in ZPS_eAplAfInit()
Can you try run JN-AN-1172 and verify that the board successfully TX RX on the highest power settings without lockup?
yes, I can build and run this program.
at first glance, there doesn't appear to be in issue in running JN-AN-1172
sorry, just saw the discussion. I eventually got it working by changing a parameter in zpscfg. But i don't have access to my code right now. Will find out which parameter that was and update here.
Hi Jia Jun Tan,
Can you confirm which JN-SW-4170 release you are using?
And are you using the DR1199 or USB Dongle binary?
Best Regards,
Mario
I am using build 1396 and the USB Dongle binary.
Hi Jia Jun Tan,
Have you made any changes?
I have been unable to replicate this issue so far. Using build 1396, and the provided USB dongle binary loaded into a JN5169 USB, I receive the following debug;
***********************************************
* COORDINATOR RESET *
***********************************************
APP: Entering APP_vSetUpHardware()
APP: Entering APP_vInitResources()
APP: Entering APP_vInitialise()
Initialising UART ...Done
BDB_vSetKeys
Recovered Application State 0 On Network 0
APP: Entering BDB_vStart()
APP: Entering APP_vMainLoop()
Best Regards,
Mario