Where to find the response data of a CLRC663?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where to find the response data of a CLRC663?

496 次查看
ME1234
Contributor I

I have an NTAG5 connected to an CLEV6630B DevBoard. After sending an Read SRAM command (0xD2) I got a card response 0x73, which is pretty fine. I could see the response data in the "Tag communication" tag of the NXP-NFC cockpit under "Card Response".  Up to there I am satisfied. Know I want to read the responsed data directly.

In which register of the CLRC663 could I find the received data? I hope to find them in FIFODATA_REG, but there I only could read 0x00 instead of the expected 0x73.

0 项奖励
回复
1 回复

452 次查看
KellyLi
NXP TechSupport
NXP TechSupport

Hello @ME1234 

Thanks for contacting us and using the NXP products.

Based on your description, there is an example based on LPC1769 MCU can be helpful to you. Please go to CLRC663 plus family | Low-Power NFC Frontends | NXP Semiconductors download the following source code and application note.

NXF92074_0-1686481341848.png

Please don't hesitate to contact us if still any questions.

BR

kelly

0 项奖励
回复