I use jn1229.
I'm going to use only the coordinator and the router to build the network. What do I need to pay attention to for the router?
When testing, I found that the transmission distance is not enough. How to solve this problem?
Hi Jun, I hope you're doing well!
You could try avoiding physical obstructions between your devices, as some materials and surfaces may reduce effective range of wireless devices.
Another thing to keep in mind is possible electronic noise and interference in the frequency range of these devices, you could try changing the connection channel to a less crowded one.
It's also worth noting that range will vary from module to module, as some of them have more powerful transceivers than others, and some even have a Power Amplifier to further increase communication range.
Please let me know if you need more information.
Best regards,
Sebastian
I need your help
I use 1229 and jn5168001m03 .
Transmission distance is less than 10 meters, how to expand the transmission distance?
Hi Jun,
The JN5168-001-M03 is not a high power module, if you try to enable it using the function you describe, you'll get an error because there's no power amplifier in the module you're using:
Only the JN5168-001-M05 or M06 modules are high power capable (regarding the JN5168 variant of MCUs), so this function is only compatible with this specific variant. I have attached a document to show how to enable high power mode on the compatible modules.
I can give you the following recommendations:
Could you please try to see if these recommendations work for you?
Please let me know if you have any other questions.
Best regards,
Sebastian