What is the default radio power of the JN5169?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the default radio power of the JN5169?

跳至解决方案
849 次查看
qingshuzhuang
Contributor II

Hello everyone:

   I need help, this may be a simple question, but I am not finding the answer.

My environment:

   JN5169

   JN-AN-1219-Zigbee-3-0-Controller-and-Switch

标记 (2)
0 项奖励
1 解答
715 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Qingshu Zhuang, I hope you're doing well!

 

By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.

 

Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

在原帖中查看解决方案

1 回复
716 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Qingshu Zhuang, I hope you're doing well!

 

By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.

 

Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.

 

Please let me know if you need more information.

 

Best regards,

Sebastian