Hello everyone:
I need help, this may be a simple question, but I am not finding the answer.
My environment:
JN5169
JN-AN-1219-Zigbee-3-0-Controller-and-Switch
Solved! Go to Solution.
Hi Qingshu Zhuang, I hope you're doing well!
By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.
Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.
Please let me know if you need more information.
Best regards,
Sebastian
Hi Qingshu Zhuang, I hope you're doing well!
By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.
Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.
Please let me know if you need more information.
Best regards,
Sebastian