WCT-5W1COILTX wireless charging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WCT-5W1COILTX wireless charging

1,416件の閲覧回数
lwwl
Contributor II

Hello everyone:
I am debugging 5W wireless charging equipment WCT-5W1COILTX, the software version is WCT1000_A11_V3.3. In order to see the debug information, the serial port and development board test points TP40, TP41 are connected (Figure 1), in the main program loop to add the following code (Figure 2), but the PC side received garbled. Who can tell me what is going on? How to communicate with the host?

0 件の賞賛
返信
4 返答(返信)

1,224件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

To communicate the WCT-5W1COILTX to the PC, NXP provides a SW package to modify WCT_A11 functions (WCT1000_A11_V3.3). You can download it from the following link: https://www.nxp.com/support/developer-resources/reference-designs/wct-5w1coiltx-single-coil-wireless...

 

Users can modify the system parameters or configurations to maintain system functionalities. For example, when either the Tx coil or main power components are changed, the user should calibrate to start the FOD. The WCT1000 A11 Reference Design System User’s Guide document describes the basic debugging environment on WCT1000. Please check section 6 of this document: https://www.nxp.com/docs/en/user-guide/WCT1000SYSUG.pdf

 

Tx board debugging uses CodeWarrior and the FreeMASTER tool.

 

Regards,

Jose

NXP Semiconductor

0 件の賞賛
返信

1,224件の閲覧回数
lwwl
Contributor II

How to make WCT and PC communicate via uart? Anyone have a good idea?

0 件の賞賛
返信

1,224件の閲覧回数
lwwl
Contributor II

No one answered

0 件の賞賛
返信

1,224件の閲覧回数
lwwl
Contributor II

nxp technical support please answer

0 件の賞賛
返信