Unable to program flash on TWR-KW24D512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to program flash on TWR-KW24D512

888件の閲覧回数
calvinjohnson-b
NXP Employee
NXP Employee

While trying to flash twrkw24d512_thread_router_eligible_device on  TWR-KW24D512, I'm getting an error complaining "protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set and mass erase is disabled". Not sure what can be done. Please help.twr_kw24_flash_protect.jpg

0 件の賞賛
返信
1 返信

660件の閲覧回数
calvinjohnson-b
NXP Employee
NXP Employee

The issue was with the connector used. Problem resolved after installing driver from P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...  

USB was used to debug.