Hello,
I imported JN-AN-1218-Zigbee-3-0-Light-Bulb (version 1008) but I am unable to build the project.
I'm getting the error:
make: *** No rule to make target `all'. Stop.
When I check the option "Generate Makefiles automatically" then I get error:
../ExtendedColorLight/Source/App_ExtendedColorLight.c:38:21: fatal error: zps_gen.h: No such file or directory
The SDK is version JN-SW-4170 Zigbee 3.0 v1840
What could be wrong with my settings/configuration?
Kind regards,
Jacco
Solved! Go to Solution.
So i figured it out.
I unzipped the AN file in my downloadfolder and imported the project.
But what i should have done is unzip the AN file in my workspace folder and then import conformBeyond Studio Common Errors bullet 2.
Then I my case change paths under properties.
Now it builds OK.
Thanks Mario for pointing me in the right direction
Regards,
Jacco
Hi Mario,
I did look at that document.
But, I must say it's not entirely clear to me.
The Wrong Path bullet isn't exactly giving a solution.
My path is P:\NXP\bstudio_nxp\...
Changed all references from C to P but that doesn't do the trick.
I have another project that builds ok. It's based on JN-AN-1171-ZigBee-LightLink-Demo and JN-SW-4168 v1620.
Yes, i did unzip the AN and removed the folder JN517x before importing. Also followed bullet 2. Same error and the project isn't in the workspace folder.
Regards,
Jacco
So i figured it out.
I unzipped the AN file in my downloadfolder and imported the project.
But what i should have done is unzip the AN file in my workspace folder and then import conformBeyond Studio Common Errors bullet 2.
Then I my case change paths under properties.
Now it builds OK.
Thanks Mario for pointing me in the right direction
Regards,
Jacco
Hi Jacco,
Please look at the next community document.
https://community.nxp.com/docs/DOC-340028
Did you unzip the AN?
Regards,
Mario