There are some issues with installing the JN5189 routines,My SDK does not match when importing the project, but I installed the 1260 documentation operation.Failed to compile.
Hi Linklai, I hope you're doing well!
Could you please try the following procedure to ensure that the Application Notes compile successfully?:
First, the Application Note's Makefile needs to be changed for the corresponding chip:
# Set specific chip (choose one)
#JENNIC_CHIP ?= K32W061
#JENNIC_CHIP ?= K32W041
JENNIC_CHIP ?= JN5189
#JENNIC_CHIP ?= JN5188
And the toolchain path needs to be changed to your corresponding MCUXpresso Version:
# Toolchain paths
TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.2.0_4120/ide/tools
TOOLCHAIN_PATH = $(TOOLCHAIN_DIR_PATH)/bin
The MCU Settings must be configured to use the JN5189 driver:
In the project's settings, please add the following build command to the options:
DEBUG=HW
Like so:
And finally, the compiled .axf file needs to be selected in the debug configuration:
Note: Be sure that the JP4 and JP7 are shorted as 3-4 on the board.
Please let me know if you need any more information or have any further issues.
Best regards,
Sebastian
Installing the latest 2.6.1SDK also has this problem
Hi Linklai,
Thank you very much for your feedback.
We are taking a look at this issue, in the meantime, we recommend doing the steps detailed above to successfully compile the application notes.
Best regards,
Sebastian
After I updated the latest routine, there was still a problem in the last step of compilation. Is this due to the unsuccessful installation of Python?