Test Waveform for IW612

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Test Waveform for IW612

688 Views
Mardin
Contributor I

Hello Friends

I have a project and using u-Blox module to be our connectivity,

We are trying to test Thread Rx sensitivity with Litepoint tester but no waveform available so far,

Coz the PHY layer is same with Zigbee, so I have ever tried Zigbee's waveform, it still failed,

Can somebody share your Thread Waveform ?

Thank you ...

 

0 Kudos
Reply
9 Replies

638 Views
Mardin
Contributor I

Hi @shaun_wu 

Below screenshot is the labtool command what we used, 

You can see no packet has received,

I attached the waveform as well, the waveform can be captured by IQxel's SA,

We use labtool to generate Tx then record it, Litepoint helps us to transfer it to IQVSG file, 

Thanks ...

 

 

thread rx.JPG

0 Kudos
Reply

677 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @Mardin 

 

We have co-operation on 802.15.4 rf test with LitePoint. LitePoint design a zigbee test file to us, you could contact them to get the waveform file. We don't have Thread file as well. Please use Zigbee waveform to test. If still not work, you could bring you fail logs and test steps to us.

 

Best Regards

Shaun

0 Kudos
Reply

671 Views
Mardin
Contributor I

Thank you Shaun

Actually we have asking LP for Thread waveform, they said no thread waveform can be provided, we have ever using buit in Zigbee waveform of LP tester, our u-Blox module still can't receive the Zigbee waveform successfully, that's why I here asking for support ...

0 Kudos
Reply

648 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @Mardin 

 

Thanks for your feedback. Could you share your test steps and labtool ouput to us?

 

Best Regards

Shaun

0 Kudos
Reply

629 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @Mardin 

 

Have you issued this commend: 

59 1 0xface 0xabcd 0xef12

following by cmd 32?

 

Best Regards

Shaun

0 Kudos
Reply

624 Views
Mardin
Contributor I

Hi @shaun_wu 

Yes, we issued the command after cmd 32, but still can't receive any packet,

Thanks ...

0 Kudos
Reply

614 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @Mardin 

Could you refer to following image to check your setup? Especially LitePoint side.

zigbee_rx_Test.png

You could also check following things:

Issue cmd 88 to check whether interface enabled successfully.

Double check the cable is good.

 

Best Regards

Shaun

0 Kudos
Reply

606 Views
Mardin
Contributor I

Hi @shaun_wu 

We have tried all waveform on-hand, can't receive any packet, could you please share the waveform what you using ? 

Thank you ...

Image (2).jpg

Image (3).jpg

  

擷取.JPG

0 Kudos
Reply

599 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @Mardin 

 

I sent you email. Please also double check mfg_tool version, if not the newest one, please use newest version to test: https://www.nxp.com/webapp/Download?colCode=NW61X2.0.0.3-18.80.2.p66.15.LABTOOLBRG&appType=license

 

Best Regards

Shaun

0 Kudos
Reply