Suggestion for selecting Wifi opencpu soc microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggestion for selecting Wifi opencpu soc microcontroller

1,320 Views
Jameson
Contributor I

Hi 

    I'm looking for a WiFi OpenCPU SoC Microcontroller with 2*UART and I2C with SD card support. Can you please suggest me an IC for my requirement.

0 Kudos
12 Replies

1,277 Views
cdoumenc
NXP Employee
NXP Employee

Hi,
If you are looking for what we call a "Wireless Microcontroller Hostless Product" (Wireless MCU with Integrated Radio), then you should have a look at table Wireless MCUs Hostless.
For instance, if you are looking for a 802.11n (Wi-Fi 4) Wi-Fi® Microcontroller SoC, you should select wifi only product 88MW320/322

0 Kudos

1,268 Views
Jameson
Contributor I
Hi
It is the latest SoC 88MW320/322.I need a latest or updated SoC microcontroller with my specification i needed.These all me parameters i needed.can you please suggest an IC for all my requirements.
0 Kudos

1,251 Views
cdoumenc
NXP Employee
NXP Employee

Hi,
On product page 88MW320/322, if you check datasheet 88MW320-88MW322 - Wireless Microcontroller - IEEE 802.11n/g/b - Data sheet (public), you will see that it supports 3 x UART, 2 x I2C and MMC4 SDIO.
To ease integration, you can choose a module among Partner Modules.
But this product supports only wifi 4 (802.11n).
Isn't it better for you to have wifi 6 (802.11ax) ? If yes, then you need product RW610 which also supports bluetooth 5.3, SDIO 3.0 and can be configurated to support at least 2 x UART and 1 x I2C.

So the 1st question is : do you need wifi 4, 5 or 6 ?

0 Kudos

1,233 Views
Jameson
Contributor I
Hi
I need wifi 6. RW610 supports alexa,azure and mqtt
0 Kudos

1,201 Views
cdoumenc
NXP Employee
NXP Employee

Hi,

I understand you have chosen RW610 for your needs, right ?
Do you need 802.15.4 ? If yes, RW612 is the one you need.
Also, I undestand you prefer using a hostless product (including an application CPU (Arm Cortex-M33 here for RW610)) instead of an IoT Product such as IW611 combined with a i.Mx host . Right ?

0 Kudos

1,195 Views
Jameson
Contributor I
Hi
Can you tell me the specification of IW611.This controller will satisfy all my requirements.
0 Kudos

1,191 Views
cdoumenc
NXP Employee
NXP Employee

Hi,
The best for you is to check dedicated page https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5ghz-dual-band-1x1-wi-f...

3 other wifi 6 similar IoT products are also available and you can see their differences here for a better comparison : https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4:WIFI-BLUETOOTH?tid=vanwifib...

 

0 Kudos

1,115 Views
Jameson
Contributor I
Hi
In the above link I didn't see that it does support i2c,Uart communication.And in additon operating system is linux and RTOS.can you please explain me that thing.
0 Kudos

1,073 Views
cdoumenc
NXP Employee
NXP Employee

For instance, if you choose IW611 (in charge of wireless connectivity), you can connect it to an i.Mx application processor (https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces... as recommended on page https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5ghz-dual-band-1x1-wi-f...

The Application Processor is in charge of i2c and uart connectivity.
Page https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4:WIFI-BLUETOOTH?tid=vanwifib... also says that IW611 can be driven by RTOS, Linux or Android OS running on the Application Processor side (ex : i.Mx).


So, I think the best thing for you is to choose on this page one partner module which includes IW611 and the corresponding manufacturer (ublox, CEL, Murata or AzureWave) will help you to use it together with the application processor.

0 Kudos

924 Views
Jameson
Contributor I
Hi
Thanks for the kindly information.I will get back to you soon for further queries about the product.
0 Kudos

1,292 Views
Jameson
Contributor I

Hi 

   Yes i have already checked the page but i'm little bit confused to select. And i have to add some information for my product. It does have alexa integration,azure and aws.

0 Kudos

1,296 Views
cdoumenc
NXP Employee
NXP Employee

Hi,
It depends on which WiFi features and capabilities you are looking for.
Did you already check page https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4:WIFI-BLUETOOTH?tid=vanwifib... ?

0 Kudos